STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to run STM32H735 CPU in maximum frequency

I am trying to run STM32H735 in 550 MHz, i had read the reference manual so write the following code.FLASH_OPTKEYR = 0x08192A3B; FLASH_OPTKEYR = 0x4C5D6E7F; if (SYSTICK_FREQ > 450 * 1e6 && !(FLASH_OPTSR2_CUR &= FLASH_OPTSR2_CPUFREQ_BOOST)) { FLAS...

Resolved! how to use the ADC the old-fashioned way.

Hi,I need to use the STM32C011F4 multichannel ADC like I used to 20 years ago with other microprocessors. That is:Select ADC channel (0, 1, 5 or 6)Start ADC conversionWait for EOCRead ADC valueStop ADCIn this application I don't want to use DMA or In...

Gaston by Senior
  • 3044 Views
  • 6 replies
  • 0 kudos

STM32H753BIT6 controller Radiation Emission issue

Hi All,We have design schematic using STM32H753BIT6 microcontroller and as of now we have cleared all EMI/EMC tests except Radiation emission. We could able to see the harmonics of 60MHz crossing the margin.We have System clock running at 480MHz, LCD...

Tejas_P_R by Associate II
  • 2898 Views
  • 6 replies
  • 0 kudos

Resolved! How to read ADC without DMA ?????

Board: NUcleo 64-G474  I just want to read 2 channels of an ADC but am presented with a bewildering array of incredibly confusing options: Ranks, Continuous mode, discontinous mode, number of conversions, oversampling, triggers, etc, etc, etc. The em...

sgordon777_0-1710460374786.png

STM32H753 littleFS Integration

Helle everyone,I want to use the littleFS file system library that I used in my previous projects in STM32H753 Internal Flash Memory. But the fact that the block size in STM32H7 is 128K made me think a little. I normally use littleFS on 1K blocks and...

DMA RX interrupt sometimes not firing?

I have an  STM32L452 part in a system with multiple DMA and interrupt operations going on.The main problem I'm having right now is _sometimes_ I don't get the interrupt for DMA RX on UART4. Sometimes I do, sometimes I don't.I have been adjusting the ...

SKarl.3 by Associate II
  • 2466 Views
  • 4 replies
  • 1 kudos

Decoupling & Vcc Pin Configuration for STM32 MCUs

Hello Community,Reaching out to you for feedback on the attached configuration for Vcc on my new STM32 based DAQ board.My objective was to reduce the inductance to the Vcc pins of the MCU (STM32G0B0RET6 64 LQFP package). Hence I clubbed three pins:A)...

Chubs_0-1720232669364.png Chubs_1-1720234917525.png
Chubs by Senior
  • 3184 Views
  • 2 replies
  • 2 kudos