STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Register issue

I have faced this issue, all the parts of my MCU registers are null. If I press "step over" button, it goes right, but when I press "resume" button, it goes as the following picture. I notified this issue when I was implementing a LCD project. I have...

ThanhPham_0-1722433052636.png

Resolved! Which code needs to be put in SRAM4 when using LPBAM tool

I have been trying to figure out which code exactly needs to be put in SRAM4 memory region for the LPBAM tool to work. All the examples I could find only use SRAM4 and fail to explain which parts are strictly needed to be placed in that part of the m...

AKova3_0-1721211628268.png
AKova.3 by Associate III
  • 2432 Views
  • 3 replies
  • 0 kudos

Resolved! Annoying glitch on Timer Output compare channel

For a project I am using a number of timers to generate and/or monitor digital signals in a custom protocol. I stumbled upon a glitch in a timer Output Compare channel which I would like to share to find whether this is recognized and if there is a p...

LVan31_0-1722425630949.png LVan31_1-1722426553044.png
LVan .31 by Associate III
  • 2874 Views
  • 4 replies
  • 1 kudos

Regarding STM32F030 HAL_UART_ERROR_FE

I have configured the STM32F030 with DMA for RX, and when sending 0x05 from a PC, I observed 0x7d on the debugger. Upon checking HAL_UART_GetError() during reception, it showed HAL_UART_ERROR_FE. I am unsure about the cause of this issue. Could you p...

STM32H745ZIT6 ADC error

I'm encountering an issue with the ADC on my STM32H745ZIT6 microcontroller when reading voltages from a power supply. Here's the problem in detail:I'm using the ADC to convert analog voltages from a power supply into digital values. However, I've not...

MorisG_PE by Associate II
  • 8737 Views
  • 20 replies
  • 3 kudos

Resolved! LIS2DTW12 - SPI

Hi,  I am attempting to obtain readings from the LIS2DTW12 accelerometer on board, utilizing the SPI interface and an STM32F098RCT6 microcontroller.I’m accessing the ‘who_am_i’ register along with the high and low registers for the x, y, and z axes. ...

Screenshot 2024-07-29 121820.png

Resolved! STM32 not working with different Supply

Hello, My STM32G030F6P6 is working fine with the power supply from Laptops USB Port. I am just running simple I2C Scan program. When I power up the STM with charging adapter it is not able to show me the i2c scanned devices on serial monitor. I am us...

How to run STM32H735 CPU in maximum frequency

I am trying to run STM32H735 in 550 MHz, i had read the reference manual so write the following code.FLASH_OPTKEYR = 0x08192A3B; FLASH_OPTKEYR = 0x4C5D6E7F; if (SYSTICK_FREQ > 450 * 1e6 && !(FLASH_OPTSR2_CUR &= FLASH_OPTSR2_CPUFREQ_BOOST)) { FLAS...