User Activity

Hi I am using below controller in one of our designSTM32G474CET3 i would like to know minimum external clock frequency on which my microcontroller works. Also my requirement includes 1 SPI, 1 I2C and 4 ADC input sensing. I would need very minimum ext...
I am using STM32G474VET3 controller.As i am using DAC out voltage for my application.So i want to know the  DAC output stability, performance over temperature, & the temperature drift at Maximum junction temperature 150 °C.Also any other factors affe...
Hi As i am using one of TIM8 input for external BKIN pin, to detect fault for PWM shutdwon.But How to prevent this on multiple fault events.Like any cycle by cycle protection is there.
Hi, i have configured BKIN pin to detect fault for my overcurrentSo for my motor driver if this pin sense BKIN input. How much time it be will taken by my microcontroller to sense and to act to shutdown my PWM gate signalsIs it hardware glued logic t...
ADC1_IN1ADC2_IN3ADC3_IN1 As i want to measure few signals simultaneously.can i configure by this way like ADC1, ADC2, ADC 3 or Separate channels from same ADC1
Kudos from