STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Struggling with USART1/LIN interrupts on STM32F3

I have a design using USART1 on an STM32F3 as a LIN slave receiver using the old standard peripheral drivers from ST Micro.  The code is too much to post here, but I have LIN Break Detect and RX Not Empty interrupts enabled, and for some reason under...

Dazai_1-1722377807126.png Dazai_0-1722377778121.png Dazai_2-1722377884096.png
Dazai by Associate III
  • 1982 Views
  • 1 replies
  • 0 kudos

FDA903D : I2c Write procedure

FDA903D : I'm facing issue with I2C write procedure. I'm writing to the slave device (FDA903D) from my custom designed board with Infineon controller being the master device . The datasheet of FDA903D is not clearly mentioning how to do I2C transfer ...

Resolved! STM32H747 Internal Temperature Measurement and Calculation

Hello, Friends, I am using ADC(16 bit) to measure the STM32H747 Internal Temperature and VrefInt based on external reference voltage (VDDA 3.3V, Vref+ 2.5V). The VrefInt result is 1.221V, which looks good. However, the temperature result is 150C, whi...

yhplx by Associate II
  • 5408 Views
  • 7 replies
  • 1 kudos

Newbie trying to Blink w/STM32H750B-DK

Hello,I acquired the STM32H750B-DK development board. Initially, when I connected it to my PC, it would power on with a display and interface. However, for the past month, it no longer turns on at all. When I connect it to my PC, a folder opens with ...

jean3 by Associate
  • 1256 Views
  • 1 replies
  • 0 kudos

PWM and ADC conflict

Hello, I'm new to STM32, I bought a Nucleo board with a STM32F334R8T6I want to generate a PWM of 10kHz and read some data in ADC channel, unfortunetely, there some conflicts between this two and I can not generate a PWM with more than 5kHz.I need som...

Nakata by Associate II
  • 3249 Views
  • 6 replies
  • 0 kudos

Resolved! H723V + HS ULPI possible damage

I am currently working on a H723 based HS USB device with external USB PHY (USB3320,USB3340,USB3300 tested).While testing i have noticed that seemingly randomly between debug/flash cycles HS USB stops working with usually no activity on the bus but t...

Ultrawipf by Associate II
  • 2745 Views
  • 4 replies
  • 0 kudos

Resolved! U585 failure to configure voltage scaling

Hello,I'm looking for some troubleshooting advice. I saw a few tickets regarding this kind of problem and confirmed that __HAL_RCC_PWR_CLK_ENABLE() is called before setting the initial voltage scaling. This test code is completely auto-generated from...

EC.3 by Associate III
  • 1323 Views
  • 1 replies
  • 0 kudos

Resolved! Differential ADC in stm32h7

I have recently purchased an STM32H753ZI board and want to configure the differential ADC to read signals directly from a function generator. I have configured it based on the following setup, but I am facing several issues with the output.Issue 1: I...

Transferring data from JPEG decoder to DMA2D directly

Hi there, I am writing a custom video decoding app that process custom stream JPEG frames from USB, without any standard on a STM32H747.So far, (more or less) so good, I use CM4 for USB operations, and CM7 for JPEG decoding and DMA2D pixel conversion...

Me2 by Associate
  • 1107 Views
  • 0 replies
  • 0 kudos