cancel
Showing results for 
Search instead for 
Did you mean: 

HRTIM interrupt callback function

JLope.11
Associate III

I would like use HRTIM timerA interruption event, so I where looking for the weak function to rewrite it but not found it.

I found that I must set compilation flag USE_HAL_HRTIM_REGISTER_CALLBACKS to 1 and make all functions as weak.

 

If I make so strong decision I disturb working that timer?,

what is the way to set the compilation flag using cubeide?

Is this the function that I must rewrite?

 

void HRTIM1_TIMA_IRQHandler(void)
{
	//USER CODE
}

 

or I must do this?:

 

void HRTIM1_TIMA_IRQHandler(void)
{
	//user code
	HAL_HRTIM_IRQHandler(&hhrtim1,HRTIM_TIMERINDEX_TIMER_A);
}

 

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @JLope.11, sorry for the delayed answer, 

To set the compilation flag USE_HAL_HRTIM_REGISTER_CALLBACKS to 1 in STM32CubeIDE:

Go to Properties>C/C++ Build>Settings, under the Tool settings tab, go to MCU GCC CompilerPreprocessor or Symbols depending on your version of STM32CubeIDE 

Then add a new symbol USE_HAL_HRTIM_REGISTER_CALLBACKS=1

Regarding the interrupt handler function, you can either use callbacks ( void My_HRTIM_TIMA_Callback(HRTIM_HandleTypeDef *hrtim)) or not (void HRTIM1_TIMA_IRQHandler(void)).

Hope that still helps!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Sarra.S
ST Employee

Hello @JLope.11, sorry for the delayed answer, 

To set the compilation flag USE_HAL_HRTIM_REGISTER_CALLBACKS to 1 in STM32CubeIDE:

Go to Properties>C/C++ Build>Settings, under the Tool settings tab, go to MCU GCC CompilerPreprocessor or Symbols depending on your version of STM32CubeIDE 

Then add a new symbol USE_HAL_HRTIM_REGISTER_CALLBACKS=1

Regarding the interrupt handler function, you can either use callbacks ( void My_HRTIM_TIMA_Callback(HRTIM_HandleTypeDef *hrtim)) or not (void HRTIM1_TIMA_IRQHandler(void)).

Hope that still helps!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.