STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC Not Working When Using VDD for VBAT on STM32L4

Hello STM32 Community,I’m encountering an issue with the RTC on my STM32L4 microcontroller. When I connect VDD to the VBAT pin (without using a battery), the RTC is not functioning. However, if I use a battery for VBAT, the RTC works fine.Here’s the ...

Sujith by Associate III
  • 8783 Views
  • 14 replies
  • 0 kudos

Resolved! L431RC CANBUS Bootloader problem

Hello, I am a developer and I am using the L431RC chip on a custom board. I am using CAN BUS to communicate with the system, and during normal operation (via firmware), there are no communication issues,in fact, everything works quite well. However, ...

Fede by Associate
  • 1275 Views
  • 1 replies
  • 0 kudos

Delta Device Firmware Update and FOTA

Using following Setup:IDE : VS Code (NRF connect plug-in)Programmer : Stm32Cube programmerDebugger: St-linkOS: Zephyr 3.6MCU: Stm32u5 seriesBootloader: mcubootI am looking for stm32 echo system tools and libraries for the delta firmware update of the...

A Maq by Senior
  • 1623 Views
  • 1 replies
  • 0 kudos

PWM Frequency Variation Issue in STM32G0C1RET6

Hello, I am trying to vary the PWM frequency of Timer 2 in between 20Khz to 200 Khz in stm32G0C1RET6 Board.1. Whenever I change the Frequency from 200 Khz to 20 Khz, it works. but then I change it again to 200Khz it just doesn't work. my PWM line goe...

Rohit007 by Associate III
  • 1326 Views
  • 1 replies
  • 0 kudos

Resolved! I2C Gives No Output

For the life of me I cannot get the I2C pins on my microcontroller to output anything.I am using I2C1 on pins PB6 (SCL) and PB9 (SDA) on the STM32F746VGT microcontroller. The pins are hooked up to a TXS0108E level shifter that has built-in pull up re...

CCend.2 by Associate III
  • 10903 Views
  • 11 replies
  • 1 kudos

Resolved! FDCAN Bus Configuration Issue: Error at Higher Bit Rates

Hello Everybody,MCU: STM32H750XB (STM32H750DK Discovery Kit)FDCAN Clock : 40MHzI'm experiencing an issue with my FDCAN bus configuration where the node enters Error state and issue persists with any data rate higher than the nominal rate of 500 kbps....

Dev_k by Associate II
  • 4371 Views
  • 6 replies
  • 3 kudos

Resolved! STM32H7 and 10BASE-1TS

Hi folks,   I need to use setup system where is 10BASE-T1S communication. And we have stm32H7 controller, so questions is which one would better use LAN8651 (MAC+PHY) chip and do controlling of chip via SPI or chose LAN8670 (PHY) and do chip controll...

Tappi74 by Associate II
  • 4640 Views
  • 3 replies
  • 1 kudos

Space Parity Setting on STM32L010RB

I want to send data from my STM32 to another micro controller and I want to enable space parity, there is no setting to enable it, the only settings are none, odd and even. For space parity i want the parity bit to always be 0.  I am using 9 bit UART...