STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Space Parity Setting on STM32L010RB

I want to send data from my STM32 to another micro controller and I want to enable space parity, there is no setting to enable it, the only settings are none, odd and even. For space parity i want the parity bit to always be 0.  I am using 9 bit UART...

Hse and hsi clock select

I am just switching clock source to MCU in RCC_CR register by making HSEON bit of above register high and waiting till HSERDY but turnsup. But thing after HSERDY turns up when I read rcc_cr register both HSEON,HSION bit of RCC cr are at logic 1. Then...

Resolved! STM32H743 RAMECC behaviour

I'm trying to use the RAMECC monitoring subsystem on an STM32H743 but there's some behaviour I don't understand. I've read the reference manual (RM0433 rev 7) and application note AN5432, as well as some related forum posts here.If I set an interrupt...

KORourke by Associate
  • 1508 Views
  • 1 replies
  • 1 kudos

Resolved! CAN Communication - STM32F098RCT

Hi,I am currently working on a Battery Management System (BMS) and an instrument cluster. I need your assistance with some issues I’m encountering while communicating between the BMS and a custom cluster board using CAN.We have two custom cluster boa...

Screenshot 2024-10-23 114441.png