STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN interrupt on STM32G481

Hello,I am using STM32G491 FDCAN modules 1 and 2 in bare metal. While everything works perfectly on CAN2 the interrupt on CAN1 is constantly disabled. And I do not mean the flags but the actual interrupt does not fire. Each time the interrupt for CAN...

Resolved! DMA across power domain

Hello everyone, I am working with the stm32h755 and I'd like to move data from spi3 rx (D2 domain) to my AXI SRAM (D1 domain) with the DMA controller DMA1. I am a bit confused by what I am reading and I can't really figure out if this cross domain tr...

Resolved! STM32F756 use TIMER event DMA from GPIO to Memory

Hello,now I will record 32 GPIO's via DMA for the analyse. The DMA itself shall triggered with a timer.So first I have found different information to solve this. So I have tested some solution, but on the STM32F756 will it not run.My solution is: GPI...

bm2 by Associate III
  • 3121 Views
  • 9 replies
  • 1 kudos

Resolved! Advice on STM32U5 multiple timer configuration

I'm struggling with how to use the timers to achieve certain behavior and am looking for some advice. First I'll describe the purpose, then how I tried to approach it, and then why I'm stuck.I need a 32-bit timebase that counts up at exactly 48kHz an...

Custom HID on STM32F103C8

Hello Everyone,Mechanical engineer at heart, I'm still a noob when it comes to STM32 coding.I'm trying to create a macropad (later this work might lead to a joystick) for a game I use (Starcitizen).So far, i've managed to get the input for encoders, ...

Using SMPS in STM32H745 to power core and IO

The SMPS in STM32H745IIK can optionally supply a fixed 1.8V to the internal LDO and potentially some external circuitry. In my case, I have a board with a 3.3V supply, and I want to utilize the built-in SMPS to provide a 1.8V supply and 1.8V IO level...

cos by Associate
  • 1657 Views
  • 3 replies
  • 0 kudos