STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432 dynamic VDD voltage change

I'm developing a very power-saving product. The STM32L4 is a really great product for our application ! Usually I run the STM32L4 VDD at 1.8V. Operate at 3.3V only when end user configures it via USB. The problem is that I want to switch the VDD volt...

ikeken by Associate II
  • 2478 Views
  • 6 replies
  • 0 kudos

external memory loader for STM32H7S3L8H not working

I am trying to port an existing design that did not use the external memory loader into a version where I can use the external memory loader so that I can add additional code.I watched the videos and read the materials and have successfully made the ...

JBias_1-1742224464441.png JBias_2-1742224481916.png JBias_3-1742224602824.png
JBias by Associate III
  • 1306 Views
  • 2 replies
  • 0 kudos

Synchronizing STM32H745 DAC and ADC

Hello,We are using the STM32H745 dual-core MCU for a mostly-analog sensor project. The M4 core is running at 240 MHz and generating a signal on the fly that is passed to the DAC via a DMA stream in circular buffer mode. This part works great.The si...

STM32L051 replacement in LQFP32 with HSE support

Need advice selecting an STM32 device (package should be LQFP32).Want to replace an STM32L051 (LQFP32). Want similar footprint. The replacement shall use less power or equal. Must have possibility to run on an external high speed oscillator (HSE). Th...

MSipo by Senior II
  • 1557 Views
  • 3 replies
  • 3 kudos

Resolved! STM32C071 OSCX_OUT

Under what circumstances is the 32.768kHz clock signal present on the PC15-OSCX_OUT pin of the STM32C071 product?

TG32 by Associate
  • 920 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H573 VFQFPN68 exposed pad details

Hello,We are using the STM32H573 in a new project. We have designed a custom board using the 64-pin LQFP package.The MCU connects to a ethernet PHY using RMII interface.Our product has to meet strict radiated emissions levels that are 7dB lower that ...

benjacam_0-1739447131133.png
benjacam by Associate II
  • 1332 Views
  • 1 replies
  • 0 kudos

STM32L432KBU6TR SPI 16 bit mode issue

STM32L432KBU6 L432 chip, spi3, 16bit mode, 20M baud rate, spi output sclk is 16 cycles when it is powered on again after working for a period of time. Sometimes 15 cycles, sometimes 17 cycles, sometimes 16 cycles are output again. This will help conf...

Pinglei by Associate II
  • 1570 Views
  • 3 replies
  • 1 kudos

Resolved! SMPS Configuration for STM32H7

I've designed a custom board using the STM32H747I MCU, following the STM32H747I-DISCO reference design. In my design, I've connected VLXSMPS to VDDLDO, similar to the reference design. I'm currently setting up the power configuration in STM32CubeIDE ...

KAnahar by Associate III
  • 3154 Views
  • 6 replies
  • 0 kudos