STM32G474 HRTimer, Dead time And Duty Cycle
- February 9, 2024
- 2 replies
- 2023 views
Hi all!
Hoping someone can help me with this.
Right now, I have Timer A and Timer B as my main outputs; Timer A controls one set of switches in my half bridge, and Timer B controls the other half.
I have one "mode" set, where I can adjust the phase shift between the two with corresponding dead time and it works great. No issues there.
However, what I also want to implement is a form of trailing edge modulation, without having to manually adjust/move my output pins. I still want and need deadtime too.
I attached a photo showing what I'm trying to do. OUTLR and OUTLL are the two bottom switches, and OUTUR and OUTUL are the upper switches. I can kind of do it by adjusting the falling edge deadtime, but I can't adjust it to be long enough for any sort of real power control. I basically need for the trailing edge of only *one* set of PWM outputs to be changeable, *with* deadtime still included.
Is there some way I'm not aware of to do this?
Thank you!