STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432KBU6TR SPI 16 bit mode issue

STM32L432KBU6 L432 chip, spi3, 16bit mode, 20M baud rate, spi output sclk is 16 cycles when it is powered on again after working for a period of time. Sometimes 15 cycles, sometimes 17 cycles, sometimes 16 cycles are output again. This will help conf...

Pinglei by Associate II
  • 1570 Views
  • 3 replies
  • 1 kudos

Resolved! SMPS Configuration for STM32H7

I've designed a custom board using the STM32H747I MCU, following the STM32H747I-DISCO reference design. In my design, I've connected VLXSMPS to VDDLDO, similar to the reference design. I'm currently setting up the power configuration in STM32CubeIDE ...

KAnahar by Associate III
  • 3157 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F407 Discovery Board UART1 not working

I'm having the same problem on 2 different boards. I gen'd up a simple program using CubeMX and I'm only sending some data to both ports at the same time: void StartTask02(void const * argument) { /* USER CODE BEGIN StartTask02 */ /* Infinite loo...

DS1Z_QuickPrint1.png GPIO STM serial test.jpg

Resolved! SDMMC2 on STM32H755 Nucleo PB14 Reserved

Hi folks,I have SDMMC1 working on CM7 on my H755 Nucleo. Now I want to migrate FAT-FS and the uSD to CM4, in which case I think I should switch to the SDMMC2 peripheral since it's in D2 domain along with CM4.I have a some questions about this and wou...

bramble by Senior
  • 1302 Views
  • 1 replies
  • 1 kudos

USB trace impedance for STM32H725

I am laying out a USB for a STM32H725. I would like clarification on something out of the datasheet (DS13311).Note 2 under table 118 states: No external termination series resistors are required on USB_DP (D+) and USB_DM(D-); the matching impedance i...

VIR by Associate
  • 964 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-H7S3L8 USB-HS & XSPI problems

  I have several problems with the NUCLEO-H7S3L8 board   1) When initializing the USB - HS peripherals, I getting stuck in the "USB_CoreReset" function: Related problem and after some time when (count > HAL_USB_TIMEOUT) the program goes to Error_Han...

Shpegun60_0-1738247929301.png Shpegun60_1-1738251040439.png Shpegun60_2-1738251337311.png Shpegun60_3-1738251362022.png
Shpegun60 by Associate II
  • 1205 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U585 MPU cacheability?

I am using an STM32U585QI.  I have some memory mapped PSRAM that I'm using.  I have enabled DCACHE, but do I have to manually do something with the MPU for it to cache memory accesses to/from the memory?  The reference manual says:"In addition, the A...

BDoon.1 by Associate III
  • 1176 Views
  • 1 replies
  • 1 kudos

Writing and reading external parallel flash with STM32

HelloI am using STM32F103C8 and I want to read and write to CAT28F010P Flash chip.This flash chip has parallel buses for data and address. Also there are 3 control lines as CE, OE and WE.So there are 28 lines in total coming out of this chip. I was a...

VarioSL by Associate
  • 2230 Views
  • 6 replies
  • 2 kudos

Resolved! Choosing a product

Hi, I find the search system on the ST website to be lacking. There are a lot of parameters I can't search for/filter by. Is there an ST e-mail / form contact I can use to ask for help? If anyone here can help, I'll try to describe what I am looking ...

kasper8 by Associate
  • 864 Views
  • 1 replies
  • 0 kudos