User Activity

Fairly basic question; When working with CubeMX, I want to set up ADC1 and ADC2 to trigger and sample at the same time, using an HRtimer trigger pulse, at about 5 MSPS. ADC1 is sampling channel 1, and ADC2 is sampling channel 4.I have them working ri...
Hi All. So, I'm currently working on a project that I need some assistance with... I'm using the HRTimer and ADC. Timer A and Timer E both control my gate drive outputs; they're variable frequency. I also have Timer F, which controls my ADC sampling....
Hi all! Hoping someone can help me with this. Right now, I have Timer A and Timer B as my main outputs; Timer A controls one set of switches in my half bridge, and Timer B controls the other half. I have one "mode" set, where I can adjust the phase s...
Hiya!  I'm trying to figure out the clock config for my micro. I'm using ADC3 IN1 currently, and using the internal HSI clock source. Using the default settings, I can't seem to get anything better than 3.3 MSPS, and this is with a 10-Bit ADC resolut...
Kudos from
Kudos given to