STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Digital Image Processing with STM32 ?

Dear Members or ST Employee,I've been looking for inspiration from STM32 board for digital image/signal processing,Any boards that can be used for image processing straight away from development board?because I need RAM for it, and the internal RAM w...

STM32L4 VRefint dependency on temperature

VRefint is between 1.18 and 1.22V depending on temperature. As in our hardware we have termometer available i would like to know more precisely what Vrefint voltage actually is.What are exactly the relation between temperature and Vrefint voltage?equ...

WPuch by Associate II
  • 693 Views
  • 0 replies
  • 0 kudos

Implementation of filesystem

Hi i am trying to implement Littlefs filesystem on STM32L151 MCU which is interfaced with external Flash memory using SPI.is it already implemented on any one of the STM32 board? if yes-i need to know what are the key features to be carried out to im...

Rekha.k by Associate II
  • 3329 Views
  • 4 replies
  • 1 kudos

AHB and APB

Hi ST Community,I’d like to know why sometimes we use GPIO with AHB and sometimes with APB ?

idrissmc by Associate III
  • 3261 Views
  • 4 replies
  • 0 kudos

AT command for sending sms ?

Dear Members, I want to send SMS but I stack with ^z,how can I rectify it ?uint8_t aTxBuffer5[] ="AT+CREG?\r"; uint8_t aTxBuffer6[] ="AT+CGMF=1\r"; uint8_t aTxBuffer7[] ="AT+CMGS=\"61400000997\"\r"; uint8_t aTxBuffer8[] ="\"TEST SMS FROM STM32 ...

Resolved! stm32H743Y vs stm32H743V

Dear all,I am facing to a stm32h743 issue. I have a Nucleo with the stm32H743 Rev Y that work perfectly. Now, I just tried the new Nucleo equipped with the stm32H743 Rev V. As expected, my previous code (Rev Y) does not work on the new device (Rev V)...

I2C errors and interrupts

Hi there, I'm using the STM32H7 to talk to a CS2000 clock chip over I2C. I'm using interrupt mode.I'm just trying to read the chip's ID register for starters. Despite the CS2000 ACKing the first 'setup write' byte, it won't write the second byte (wit...

Mttjcksn by Associate III
  • 2836 Views
  • 2 replies
  • 0 kudos

Hi everyone, I am fairly new to ST and I'm working on a project where i need 8 phase shifted pwm signals(each phase shifted by 45 degrees and same duty cycle)

i was thinking if there is a way i could generate 4 timers phase shifted by 90 degrees wrt each other so that i could use them to generate 2 pwm signals (on each timer using asymmetric mode) . can this be done? if not, is there any other way i could ...

Vbhus by Associate
  • 1526 Views
  • 2 replies
  • 0 kudos

i2c communication on STM32F103RB

i want to read ADC MCP3425 digital data using i2c communication with Stm32f103rb nucleo-64 board . For programming of nucleo-64 i used arduino ide. 1] Is it possible to modify default setting of MCU clock ? 2]what is the default setting of i2c clock ...

vmool by Associate
  • 1037 Views
  • 0 replies
  • 0 kudos