STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

My STM32F051C6 dev board cuts the connection to Eclipse after starting to debug, i cannot get it to stay connected. This happens with all projects regardless if they worked before. Can anyone please help??

Im debugging with an ST-LINK J9357 debugger chip in Eclipse's debug workbench . I've been over the debug configurations many times and cannot find an error. Once i start the debug and it shuts off the connection there isn't even an error box detailin...

DC.18 by Associate
  • 1202 Views
  • 1 replies
  • 0 kudos

Interfacing STM32F401 with OV7670 camera: scrambled images

Hello everyone,I am trying to interface my STM32F401RE with OV7670 camera. I have set the input clock for the camera from the MCO output of the board at 8MHz. Because my board is not provided with DCMI, I have to explicitly implement the communicatio...

MCarp by Associate
  • 1217 Views
  • 0 replies
  • 0 kudos

I am using STM32L432KBU6 controller in my design. I want to Monitor battery voltage on ADC pin using Voltage divider.

LiPo battery ratings is 3V to 4.2V.Any reference circuit than please share.I want to learn exact calculation for ADC.There are various values of RAIN mention in table 63 of datasheet.Should i use same values for Resistor Divider?How much counts i can...

HRawa by Associate II
  • 1973 Views
  • 4 replies
  • 0 kudos

Resolved! Can someone identify this IC?

I would have thought the text on it would prove to be meaningful but apparently according to every search I have tried it is not. Thanks for your help.

GWilk by Associate II
  • 1750 Views
  • 2 replies
  • 0 kudos

Executing independently compiled code in RAM.

I have a device that must execute precompiled functions which are copied to a place in RAM. Function calling:PLC_main = (pFunc_main) 0x30000001; PLC_main();Compied function: PLC_1 0x30000000: 4811 .H LDR r0,[pc,#68] ; ...

VNilo by Associate
  • 1354 Views
  • 2 replies
  • 0 kudos

Temperature of the internal temperature sensor

Using STM32F0308C on a custom board. When I read the temperature sensor I am getting 1765 and the TS_CAL value is 1778.Supply voltage is 3.3V, VREF_INT is 1524 and I am reading 1525 on the internal reference. So I assume I must apply a 1524/1525 corr...

ECost by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

I am using STM32F030c8t6 in my device which is battery operated. I want to monitor a standard 3.7V Lipo battery voltage so I used a voltage divider at the battery and divider output is set to 3.3V which goes to ADC pin of Controller.

1. Is it ok to set 3.3V as a divider output which goes to ADC pin?2. The external voltage at VDDA pin (We have given the same VDD as VDDA) show some fluctuations while ADC monitoring so can you suggest the best possible way to monitor battery voltage...

HRawa by Associate II
  • 940 Views
  • 0 replies
  • 1 kudos

Mismatch datasheet reset value and reality

Dear community,I am using the STM32F103C8T6 32 bit ARM Cortex M3 microcontroller.In Section 9.2.1 in the reference manual (GPIOx Control Register Low) it says that the reset value is 0x4444 4444 (which means all pins are floating inputs).However, whe...

Xhendos by Associate
  • 783 Views
  • 0 replies
  • 0 kudos

Timers frequency divided by 2

Hello everybody!I try to configure TIM2 to interrupt in the range of 100Hz ... 1kHz. Strangely, the actual frequency I set is divided by 2: if I configure the timer to run at 1000Hz, it will run at 500HzTIM2 configuration:void System::InitTimers() ...

jean by Senior
  • 1815 Views
  • 8 replies
  • 0 kudos