User Activity

Posted on June 12, 2018 at 12:41Hi all,I have a board using the STM32F765, which uses the QSPI interface to fetch data from an FPGA. The normal sequence of operation is: A timer in the FPGA causes it to perform a sequence of events which produce a ...
Posted on March 10, 2015 at 15:05Hi, I have a design using an STM32F205. It needs the capability to be upgraded via the USART interface, and I'd like to be able to use the built-in bootloader for this purpose. My application contains a command which...