STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L073 strange behaviour after 2nd bootloader jump to app

Heyho,playing with the L073, partitioned the flash for bootloader "BL" (bank 1) and application (bank 2).No writing of app yet, just testing jumping back and forth.I just added a no-init variable for communication between BL and app, mainly to tell t...

LCE by Principal II
  • 218 Views
  • 3 replies
  • 0 kudos

STM32N6570-DK: Flashing Issue After Reset

I am currently working on the STM32N6570-DK board for a camera-based project.Development SetupIDE: STM32CubeIDE (Version 2.1.1)Tool: STM32CubeMX (with STM32N6 package installed)Issue 1: Flashing & Boot BehaviorI tested the example GPIO_IOToggle progr...

Built in bootloader jump to address

AN2606 indicates that I should be able to activate the built in boot loader by jumping to the correct address in ROM, but I can't work out what that address is for the STM32U535CB. 

psusi by Associate II
  • 296 Views
  • 6 replies
  • 2 kudos

An example for LPUART with LPDMA - STM32U575

Hello everyone,I develop a project with STM32U575 and I want to use LPUART with LPDMA, normally I use LPUART with normal DMA in my other stm32L4 projects but here I couldnt work with this peripherals. Low power is not a critical issue of this part of...

1.png 2.png
Epamuk by Associate III
  • 1761 Views
  • 3 replies
  • 5 kudos

Resolved! STM32 with at least 4x SPI and 2x USB

Dear STMicroelectronics Team,I am looking for an STM32 microcontroller for a new project. My main requirements are:At least 4 SPI interfacesAt least 2 USB interfacesCould you please suggest suitable STM32 part numbers that meet or come close to these...

DZ888 by Associate
  • 235 Views
  • 2 replies
  • 0 kudos

Issue changing clock speed via internal PLL

Hi all,We have a product using a STM32L451CEU6. We have gone through low rate initial production and it has met requirements but the customer has requested a change. We are experimenting with increasing the system clock speed the device is running at...

jramsay42_0-1774910882959.png jramsay42_1-1774910882960.png