Skip to main content
gunccc
Associate II
August 7, 2023
Question

VREFBUF Enable Problem

Hi,

I am working on STM32G474CET mcu. I am trying to use VREFBUFF voltage for ADC channel referance voltage. My configuration looks like the following. 

gunccc_0-1691414511024.png

When i run the code, it stuck in the HAL_SYSCFG_EnableVREFBUF function. Whenever i check the 'tickstart'  variable it remains 0. 

 

/**
 * @brief Enable the Internal Voltage Reference buffer (VREFBUF).
 * @retval HAL_OK/HAL_TIMEOUT
 */
HAL_StatusTypeDef HAL_SYSCFG_EnableVREFBUF(void)
{
 uint32_t tickstart;

 SET_BIT(VREFBUF->CSR, VREFBUF_CSR_ENVR);

 /* Get Start Tick*/
 tickstart = HAL_GetTick();

 /* Wait for VRR bit */
 while (READ_BIT(VREFBUF->CSR, VREFBUF_CSR_VRR) == 0x00U)
 {
 if ((HAL_GetTick() - tickstart) > VREFBUF_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }

 return HAL_OK;
}

 

When i try the same configuration on empty project, it worked fine. So i can see its not about hardware. What am i missing? 

 

This topic has been closed for replies.

5 replies

ST Technical Moderator
August 7, 2023

Hello @gunccc,

Have a look at this FAQ: How to configure VREFBUF on my STM32,

May be this post can help: 2 bugs with VREFBUF and STM32Cube on at least STM32G4

Otherwise, please share your ioc file to check the case, and precise which CubeMx et firmware package versions are you using?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
gunccc
guncccAuthor
Associate II
August 8, 2023

Hi @Imen.D . 

Thank you for your answer. Like you said 2 bugs with VREFBUF and STM32Cube on at least STM32G491 post really helped me. Like bobert said, i enabled the low impedance before Vrefbuf. And like that my code worked. But I had to interfere the STM's code. In order to use the user code section, I also had to include the enabling of the clocks in the user code. Now my MspInit code looks like that. 

void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 __HAL_RCC_SYSCFG_CLK_ENABLE();
 __HAL_RCC_PWR_CLK_ENABLE();
 HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);
 /* USER CODE END MspInit 0 */

 __HAL_RCC_SYSCFG_CLK_ENABLE();
 __HAL_RCC_PWR_CLK_ENABLE();

 /* System interrupt init*/
 /* PendSV_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0);

 /** Configure the internal voltage reference buffer voltage scale
 */
 HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE0);

 /** Enable the Internal Voltage Reference buffer
 */
 HAL_SYSCFG_EnableVREFBUF();

 /** Configure the internal voltage reference buffer high impedance mode
 */
 HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);

 /* USER CODE BEGIN MspInit 1 */

 /* USER CODE END MspInit 1 */
}

Is it okay to use it like that or is there a better way to do it? 

gunccc
guncccAuthor
Associate II
August 8, 2023

Also in using internal Vrefbuf : HAL Code generation issue post, people have used the same method as me and suggested this as a bug in HAL. 

ST Technical Moderator
August 17, 2023

Hello,

I escalated this issue internally and internal ticket (ID 159452) is submitted to be reviewed and treated.
 (PS: ID 159452 is an internal tracking number and is not accessible or usable by customers).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
July 30, 2025

Hello, 

This issue is fixed in the latest release of STM32CubeMx v6.15.

Thank you for your contribution and for having reported this issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks