User Activity

I want to use two timers: one timer to generate PWM, and another timer to generate periodic interrupt events to trigger DMA. For example, use TIM2 to output PWM, and TIM3 to periodically generate update events to trigger DMA for updating the duty cyc...
I want to use STM32CubeMX to configure the relevant peripherals and use a single timer, such as TIM3, to simultaneously implement an orthogonal encoder and input capture for frequency measurement. Can this be achieved?
"I have a project A that I haven't used for some time. During that period, I was using project B, which has been working fine. However, when I tried to use project A again, I was informed that its CMake configuration failed. Can you please tell me ho...
"After configuring a CMake project for STM32F407ZGT6 using STM32CubeMX, I imported it into VSCode, but encountered numerous errors and could not use it properly. However, projects for the H7 and F1 series work fine. What could be the issue?" 
Kudos given to