STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PA0-WKUP - do I have to care on INPUT?

I'm in need to scan a bunch of contacts in a 4 rows, 8 column diode matrix configuration. PA0-PA7 are the inputs, PB12-PB15 the outputs. What I'm wondering about is the PA0-WKUP special function in contrary to the rest of inputs (PA1-PA7). Do I have ...

STM32H755ZI custom board not detected by ST-Link

Hi community !I was working on a custom STM32 board as part of a robotics project. We started evaluating STM32H7 through the Nucleo boards, and now that we've confident with our chip selection, I designed a custom nucleo-type board, which can later b...

Aadi by Associate
  • 221 Views
  • 2 replies
  • 0 kudos

DFU mode for STM32N6

Hello, I'm reading the article on "How to create an STM32N6 FSBL load and run" and have a couple of questions about DFU implementation on the STM32N6: 1. Is DFU possible with the application as part of the FSBL? 2. Is there an example on how to imple...

Resolved! Per-device CAN buffer capabilities

Is there an easy way to find devices that support specific CAN buffer configurations?For example, some only have receive queues whilst others allow a number of receive buffers to be configured (which is what I want). I know the H7x7 supports this, bu...

CTapp.1 by Senior III
  • 219 Views
  • 3 replies
  • 3 kudos

ETM trace maximum data rate on STM32U575

Hello everyone,We are having trouble getting tracing to work with our target at full clock speed and would like to understand why, we have an application running on STM32U575 @ 160MHz CPU clock, we also connected the J-Tracer to it using a connector ...

Screenshot 2024-06-11 163220.jpg

Resolved! VDD33USB connection problem when not using USB

Hi,I do not plan to use USB, and the STM32N6's VDD is 1.8V.However, creating a new 3.3V power supply just only for the VDD33USB pin is too inefficient.The datasheet lists the absolute maximum ratings for VDD33USB as ranging from 0V to 3.6V when USB i...

Resolved! question aboue bootloader Write_Memory command

Hi, I am tring to write data by the FDCAN bootloader of system memory, my target is STM32H563. Now, I can read the device ID, perform the mass erase command, but I can't write data to SRAM/Flash, the FDCAN bootloader doesn't response any CAN message...

Snaku_0-1762338250957.png Snaku_1-1762338502807.png
Snaku by Associate III
  • 600 Views
  • 6 replies
  • 2 kudos