cancel
Showing results for 
Search instead for 
Did you mean: 

Clock confirmation in NUCLEO-F767ZI

ak52
Associate III

Hello,

I was looking into this wiki tutorial on setting up a UDP echo server by @mƎALLEm , and the clock configuration caught my eye and wanted to confirm a few things.

  1. On the nucleo board , the 8 MHz crystal (X3) is not soldered and the 8 MHz clock signal comes directly from the ST-Link MCU (U2) via SB149. I have checked this on a oscilloscope. ak52_0-1753853874258.png

But in the tutorial , in Section 2.1 Clock configuration Section , the screenshot shows the input frequency set to 16 MHz. As far i am aware this should be 8 , not 16 MHz. Can someone please confirm this?

ak52_1-1753854095962.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Super User

The current STM32CubeMX version 6.15.0 generates 8 MHz HSE clock by default.

The screenprint shows 16 MHz which is wrong, but irrelevant here as the PLL Source Mux is switched to HSI clock, not HSE.

hth

KnarfB

View solution in original post

3 REPLIES 3
KnarfB
Super User

The current STM32CubeMX version 6.15.0 generates 8 MHz HSE clock by default.

The screenprint shows 16 MHz which is wrong, but irrelevant here as the PLL Source Mux is switched to HSI clock, not HSE.

hth

KnarfB

ak52
Associate III

Thanks for the confirmation

STackPointer64
ST Employee

Hello @ak52,

Thank you for pointing this out. As @KnarfB mentioned, the HSE value in the example is irrelevant because the PLL clock source is set to HSI. However, the clock tree figure in the article has been updated to clarify this.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.