cancel
Showing results for 
Search instead for 
Did you mean: 

Designing a custom board with STM32H725ZGT3

Ironman
Associate II

I designed a custom board using the STM32H725ZGT3. The references I followed include the datasheet, application note AN5419, and the STM32H745ZIT6 Nucleo board design, among others.

 

After powering up the board, I was able to connect to it via ST-Link using STM32CubeProgrammer, and successfully uploaded a simple blink code using STM32CubeIDE. The code worked, and the LED started blinking.

 

However, after a power cycle (i.e., turning the main power off and on again), the board stopped running the code, and the LED no longer blinked. I tried reconnecting with STM32CubeProgrammer, but I received a "Target not found" error.

 

After that, I connected the BOOT pin to 3.3V. This allowed me to connect to the board again using STM32CubeProgrammer, but I couldn’t upload code using STM32CubeIDE. I then changed a setting in the CubeIDE:

 

System Core → RCC → Parameter Settings → Power Parameters → PWR_LDO_SUPPLY

 

After this change, I was able to successfully upload the code. However, the LED no longer blinked as before. I tried connecting the BOOT pin to ground again, but it still didn’t work.

 

My Questions:

 

Is my schematic correct?

 

Is the MCU damaged?

 

If the code uploads successfully and the board connects, why is the LED not blinking? Could it

be a power issue?

1 ACCEPTED SOLUTION

Accepted Solutions
Ironman
Associate II
4 REPLIES 4
TDK
Super User

PDR_ON should be tied to VDD.

VCAP caps should be 2.2 uF, not 0.1 uF.

 

I doubt anything is damaged.

If you feel a post has answered your question, please click "Accept as Solution".
LCE
Principal II

I'm using the programming connector always with NRST.

Measure the voltage at VCAP, it should be close to the VOS you set (1.x V).

 

FBL
ST Employee

Hi @Ironman 

You might be able to recover your MCU by selecting power down mode or under reset while connecting to CubeProgrammer if it is stuck due to incorrect power configuration.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Ironman
Associate II

Thank you all

I finally I got the solution from 

https://community.st.com/t5/stm32-mcus/unable-to-connect-to-stm32h7-devices/ta-p/49296

It worked for me