STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 UART Rx with unknown length

hi i have a problem with my uart program the thing is i have to determine the buffer size of the rx i'll call it rx_buff now i have multiple reception well different messages sizes some times 50bytes some times 2bytes but the problem is that when sen...

bakhti by Associate II
  • 1654 Views
  • 2 replies
  • 0 kudos

STM32H743 – DAC with DMA not working ?

Dear Reader,In this project we’re required to output a DAC signal (to begin with a sine-wave would suffice in terms of proving the code) on PA4 of our STM32H743 micro using DMA.I’ve done some evaluation and testing based on STM’s sample project NUCLE...

TMA1of3 by Associate III
  • 1364 Views
  • 1 replies
  • 0 kudos

STM32F103c8 bxCAN Transmit Problem.

I am tried to send a simple message over CAN, but I got the broken Frame when transmitting, I capture it on a Logic Analyzer(Pic Below), it seems that it is Transmitting but not Correctly.Did I did somting wrong or Did I miss Someting?And here is my ...

0693W00000SvvccQAB.png

What happens when you press reset?

I know when we press the reset in keil or when reset happens the PC should start at 0x000...ideally in my projects and flash is remapped to the start address.But for me when I press reset it is going somwhere to 0x1ffff some stupid thing.And I'm unab...

0693W00000SvvCKQAZ.png
Vmere.1 by Senior
  • 2658 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F103 - IAP (In Application Programming) - Clock and Speed?

Currently have a STM32F103 running HSE + pll with a SysClk of 72 mhz.I want to use one of the upper flash memory blocks for storing application information - which means I need to erase and program the flash memory from my application (I do this all ...

Joe.H by Senior
  • 4311 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F746ZG JTAG Connection Failed

Hello, I have two Nucleo-STM32F746ZG development boards daisy-chained together via their JTAG pins (refer to below diagram). When connecting a JLink Plus debug probe to the microcontrollers and attempting to debug the second development board in the ...

0693W00000QL99NQAT.png 0693W00000QLAqNQAX.png