2022-02-23 11:29 AM
Hi,
This was part of another (unrelated) thread which did not get timely attention.
Prototype sketch:
Cube programmer screenshot:
CubeMX ioc file attached.
The PCB manufacturer allows window of one week to submit a modified prototype within the same quotation. Please note I'm software developer new to hardware design.
BR
2022-02-23 12:11 PM
Have not looked at your schematic. However, try using the older version of CubeProgrammer, STSW-LINK004 and see if that connects. If not, you probably have board error.
2022-02-23 1:13 PM
Hi,
Thank you @Terrance Parker , it still persists
2022-02-23 1:19 PM
I don't expect the IOC file is going to shed much light on this.
H7 not F7 per title I'm assuming.
Dead-in-the-water tends to suggest power issues.
Check voltage present on NRST and VCAP pins, along with VDD, VDDA
Check part orientation.
Check net-list for floating/disconnected power/ground islands, or mismatched net names.
With BOOT0 high cycle the power on the whole board several times, and then attempt to connect with ST-LINK.
Any other signs-of-life?
Does USB connectivity work with BOOT0 HIGH, what about UART1 reponsiveness to 0x7F data pattern at 9600 8E1 ?
2022-02-23 1:43 PM
From your schematics, it seems that you are using "SMPS supplies LDO (No External supply)", correct? if so, make sure "System supply configurations" is set for the same.
2022-02-23 1:59 PM
correction: ... if so, make sure "System supply configurations" is set for the same in CubeMX.
2022-02-23 7:39 PM
Hi @Community member
It is H7., VCP,VDD,VDDA, NRST are 3.3v
"Check net-list for floating/disconnected power/ground islands, or mismatched net names..."
Do you mean in the schematics?
'With BOOT0 high cycle the power on the whole board ...' How do I do that?
USB power is not working in all cases. 3.3v is sourced externally through board pins.
2022-02-23 7:41 PM
Thank you @Community member
How do you do that in CubeMX? Which category?
2022-02-24 5:20 AM
No, a net-list is a connectivity list exported by the schematic tool, and used the PCB tool, and usually part of the DRC (Design Rules Check), describing all the net names, and the points/nodes to which they connect.
For example your GND Triangle symbols, some have GND label in TEAL, others don't. There should be a single "GND" net in the net-list, not one call "GND" and another called "UNK". Inconsistency often leads to multiple nets which lack the connectivity that is expected.
https://resources.altium.com/p/understanding-your-pcb-netlist
2022-02-24 7:54 AM
@Community member Thank you for the advise.
I've unchecked the visibility of GND on one , and it seems that one was copied several times. DRC was checked before sending to the manufacturer. Important takeaway from your message, I should always implement a serial port, which I've under-estimated its debugging capabilities. Unfortunately, I'm still at loss.