cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link V2, STM32F103, STM32CubeIDE Debugger Error "undefined debug reason 8 - target needs reset"

Enour.1
Associate III

I'm getting debugging Error "undefined debug reason 8 - target needs reset" with ST-Link V2, BluePill (STM32F103) & STM32CubeIDE, debugger config. is "ST-Link OpenOCD", Although STM32Programmer download & run with same ST-Link V2 without any problem.

Also same STM32CubeIDE debugger is working correctly when BluePill is replaced with H743 Board, here is the result with the BluePill :

Open On-Chip Debugger 0.11.0+dev-00438-ga75fc63 (2021-11-03-15:27)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J39S7 (API v2) VID:PID 0483:3748

Info : Target voltage: 3.251665

Info : clock speed 5 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x2ba01477

Info : STM32F103C8Tx.cpu: Cortex-M3 r2p1 processor detected

Info : STM32F103C8Tx.cpu: target has 6 breakpoints, 4 watchpoints

Info : starting gdb server for STM32F103C8Tx.cpu on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : device id = 0x20036410

Info : flash size = 64kbytes

undefined debug reason 8 - target needs reset

Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1552 ms). Workaround: increase "set remotetimeout" in GDB

O.K.

O.K.:0xE00FFFD0

shutdown command invoked

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User
Enour.1
Associate III

Yes, I noted that.