STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN Communication: Can't Receive Message

I am attempting to use my STM32H7B3I-EVAL evaluation board to send and receive CAN communication messages. I am communicating with a Vector CANalayzer (16.0, VN1630A). The CANalyzer is being used both to display messages received from the evaluation ...

0693W00000Svp2xQAB.png 0693W00000Svp3MQAR.png 0693W00000Svp2BQAR.png
KMew by Senior III
  • 4373 Views
  • 9 replies
  • 0 kudos

STM32F405 bxCAN form errors

I've got a weird situation.We've got a CAN bus going between our controller and a CAT ECU with a couple of PCs watching the conversation going by at about 80 messages per second and we can get a couple of million packets with zero errors. (That's not...

Resolved! Receive parallel data in Nucleo_H743ZI2

HiI am following the AN4666 document to receive parallel gpio data, with on clock input.this is the code I wrote : I was expecting to receive gpio data and save to memory by triggering the DMA at every rising edge my issue is that the timer (input ca...

AElta.1 by Associate II
  • 1354 Views
  • 1 replies
  • 0 kudos

STM32 UART Rx with unknown length

hi i have a problem with my uart program the thing is i have to determine the buffer size of the rx i'll call it rx_buff now i have multiple reception well different messages sizes some times 50bytes some times 2bytes but the problem is that when sen...

bakhti by Associate II
  • 1647 Views
  • 2 replies
  • 0 kudos