STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does the baud rate get shared if I use two or more UARTs?

Hi! I am discovering the world of STM32 and currently using a STM32F4 to establish a UART communication (send and receive data). I wrote a pretty basic program to send and receive a message (basically a loop) with a baud rate of 9600. The users manua...

LimoGr by Associate II
  • 2584 Views
  • 2 replies
  • 0 kudos

About example source code for stm32H747I-EVAL

HiI am trying to test STM32H747I-EVAL and LCDMy questions are as belowsAre STM32H747I-EVAL and LCD connected with RGB Connector? ( I want to connect each other with RGB connector when I design a circuits for STM32H747 with LCD) I ...

STLINK-V3MODS dedicated firmware for UART bridge

I'm considering using STLINK-V3MODS for RS-485 via VCP. For it I would need DE (Driver Enable) functionality. (Something similar was commented in an old question)In the user manual, when UART bridge is described it says:"UART signals with hardware fl...

jovijuan by Associate III
  • 1350 Views
  • 1 replies
  • 0 kudos

Change Uart baud rate on the fly with cube?

Posted on September 18, 2017 at 16:07I see that this has been asked a few times with no real resolution or workaround, so I'll ask again please?I have USART3 configured at 9600 Baud. I test this with a terminal program also set at 9600 and it works ...

nibbly78 by Associate III
  • 4499 Views
  • 8 replies
  • 1 kudos

STM32H750IBK6 REV V sample what is max FMC CLK we can run SDRAM the datasheet says 2 different values for rev V and REV Y IC revision what is safe area of operating FMC CLK with SDRAM

STM32H750IBK6 REV V sample what is max FMC CLK we can run SDRAMthe datasheet says 2 different values for rev V and REV Y IC revision what is safe area of operating FMC CLK with SDRAM

Ssaga.1 by Associate II
  • 4108 Views
  • 7 replies
  • 0 kudos

bno055 with stm32

I wanted to see if the bno055 sensor is ready and set the PB8, PB9 pins as SDA, SCL. (my mcu = stm32f334r8)connectionsSDA_pin -> SDA pin sensorSCL_pin -> SCL pin sensorVCC -> VCCGND -> GNDbut the variable is never HAL_OKthanks for answer.

0693W00000aI7CEQA0.png
Loodan22 by Associate II
  • 6622 Views
  • 8 replies
  • 0 kudos