User Activity

Hello everyone,I've spent a considerable amount of time trying to change the default AES and ECDSA (ECCKEY1) keys, but I can't figure out why it always results in a 'Fw header authentication error' during the firmware image update process.The project...
I have the latest X-CUBE-SBSFU package and STM32CubeIDE 1.13.2. Building the SECoreBin project has failed with 4 errors and 4 warnings. It looks like several others experienced the same issue with different example projects.Here's the output of the c...
The following two designs were generated by EDS: Could someone please advise which one is more recommended for powering a LED strip? And can you suggest any off-the-shelf transformer PN that can go with any of these designs?
Hello everyone! I was wondering what might go wrong with I2S DMA configured in normal mode for audio streaming with double-buffering technique. I'm not talking about circular buffer here (ping-pong) where a single buffer is used in halves in HC and T...
I believe all of the audio processing addon libs, (SRC236/SRC441) are built without hardware FPU support. The problem is my entire project was built with hard FPU support. I tried the mixed SW/HW, but that didn't solve the issue and I couldn't build ...