STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103C6T6 Flash Size is incorrect reporting 32 and not 64

stm32cubeprogrammer v2.13.0 reporting incorrect sizeAs is st-infoFound 1 stlink programmersversion: V2J41S7serial: 6600240013000039544B524Eflash: 32768 (pagesize: 1024)sram: 10240chipid: 0x0412descr: F1 Low-density deviceI am on ubuntu 23.04Any help ...

bibble235_0-1687093691011.png
bibble235 by Associate III
  • 1883 Views
  • 2 replies
  • 1 kudos

SAI DMA circular mode

I'm working on the SAI part to read the ICS4342MIC through I2S protocol, and looking for a way to stream a large amount of data from the microphone to the hyper ram (in memory mapped mode). The current available feature of the HAL_SAI_Receive_DMA fun...

VPHAM.1 by Associate
  • 1879 Views
  • 2 replies
  • 1 kudos

STM32WL55 - ADC conversion time

Hello everyone!I'm working on STM32WL55JCI7 board and trying to run ADC at the fastest speed (min total conversion time mention on datasheet 0.4uSec) and I don't receive this time.My configuration is the following:And to measure total time of convers...

MichaelMor_0-1687075081305.png MichaelMor_1-1687075306648.png

Resolved! Debugging STM32f405 using Nucleo board .

Hello Team,I debug STM32F405 on my custom PCB using nucleo board and STLink utility software.Now, I have added a digital isolator on my PCB , and the STM32F405 MCU is powered by the isolated  3.3v supply & ground  of the isolator.Now, the Nucleo boar...

SMour.2 by Associate III
  • 2854 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with UART communication functions.

All these functions have one problem, let's say in this function HAL_UART_Receive_IT(&huart4, data,5);the third parameter is the number of transmitted characters.If you enter more or less characters in the COM port of the terminal than specified in t...

MMust.5 by Senior II
  • 2801 Views
  • 2 replies
  • 0 kudos

Can HAL_CAN_AddTxMessage Not Transmit.

Hi I try to send a message to the CAN interface, use HAl functionHAL_CAN_AddTxMessage.But the message not send.I verify with debug that the interface is allwais in Listering HAL_CAN_STATE_LISTENING.Do you have idea what is wrong?uint8_t CAN_TX(int16_...

PZamb.2 by Associate III
  • 1979 Views
  • 1 replies
  • 0 kudos

UART information missing from RefMan, HAL_UART_Init() error

I found this problem with STM32L476 but I suspect it may be a general STM32 quirk.The manual does not list the minimum and maximum value of UART BRR register. While the minimum value of 0x10 seems to be quite obvious, the maximum correct value in the...

gbm by Principal
  • 1744 Views
  • 0 replies
  • 2 kudos