hi,I am trying to connect ili9341 - STM32F722ZE FSMC- TFT but i couldn't succeed .ili9342 16bit - is working in direct GPIO 16 bit data PORT drive with STM32F722ZE not in FSMC-TFT . Looks most of the ili9341 working with FMC-TFT STM32F4 Series aro...
hi1. STM32F722ZE & Winbond SDRAM is working fine with follow setting .W9825G6KH-6I 166MHz/CL3 or 133MHz/CL2 CASLatency = FMC_SDRAM_CAS_LATENCY_3; SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_3;my understanding was MCU main clock was divide by 2 is made o...
hi ,Working on USB - Device_Only wake up from Stop mode and entering to stop mode is successful but not wakeup from stop mode .There is no example code for USB wake up from STOP Mode .Entered to stop with following code : HAL_SuspendTick();
HAL_PW...
hi all and @waclawek.jan @Lubos KOUDELKA USB - HID -Keyboard is working fine and keycode coming properly . Enter to STOP mode is successful by HAL_SuspendTick(); HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);Trying to wakeup fro...
hi,USB keyboard working fine via HID and i need have small Manual Keyboard Detection by pressing button . it's not compiling if( HAL_GPIO_ReadPin(GPIOC, button_Pin))
{
if(USBH_HID_GetDeviceType(USBH_HandleTypeDef *phost) == HID_KEYBOARD)...
hi,i was used stm32f446re . Using ULPI interface for HS operations on STOP Mode will be solution . ( not USB related )Currently working on stm32f722ze and going to add stm32h7b0 power saving is essential in any series . Hope your suggestion will...
hi , i need add few more points on this subject .G Series ,H5 series, L5 Series , U5 Series controller having low power option in host mode but there is NO USB wake up interrupt call . these controller having Type C option as per cubemx .USB HOST +...
hi , I do agree i need to manage this . it may be crazy but I try use Device_only low power code in HOST_only mode but some typedef are some functions are different for Host _only Mode .this is just a request if share me small code of Host_Only low ...
Device_Only Mode having low power option !!!!!!! but as you said Host_Only mode is suspend the low power option . even i have with checked Cube Mx separately and they also behave same condition . Kind Request : can you please confirm me HOST + HID ...