cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G474 HRTIM single-shot reset trigger source other than HRTIM external events

JRyu.1
Associate

Hi,

I could generate a single pulse to the HRTIM CHA1 by using HRTIM EEV6 (I tried with EEV1, but it did not work).

Is it possible to generate a single pulse by using other high-resolution timers or timers? In the CubeMX, timers can be selected as a reset trigger source in the Reset Trigger Sources Selection. I tried it with the HRTIM master timer, but it did not work for me. I read the HRTIM Cookbook, and the "Multiphase buck converter" example describes that single-shot re-triggerable mode is used with the master timer, so I assume that it should work.

Is there an example project/code for me to try with?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JRyu.1
Associate

I found that I did not start the master timer. It works now.

View solution in original post

1 REPLY 1
JRyu.1
Associate

I found that I did not start the master timer. It works now.