STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Calculate caps for LSE crystal oscillator

hi,i am using a ECS-.327-9-34QCS-TR with a 1.5pF caps on a STM32H743BIT6.I want to know the exact method to calculate the right value for the oscillator caps.because my RTC is off by 5mSec.

DS18B20 Match Rom command fail

Hi. I'm using STM32F030C8T6 MCU to communicate with multiple DS18B20. I'm using Timers to make 1us delay. I set my prescaler to 48-1. and I'm running on 48MHz clock. when i connect two sensors to my MCU, i can't read temperature, so for testing i dis...

MNoro.2 by Associate II
  • 2063 Views
  • 2 replies
  • 0 kudos

Resolved! stm32c011 in-application option byte programming

Good morning,I'm trying to program the user option bytes of the STM32C011 using the HAL. The objective of the test is to toggle the BOR bit.  static HAL_StatusTypeDef testOptionBytes() { FLASH_OBProgramInitTypeDef obInit = {0}; FLASH_OBProgra...

AndreasS by Associate
  • 1571 Views
  • 1 replies
  • 0 kudos

Vrefint and Vts very noisy with SAI active on G4

We are using an STM32G491 with TDM audio output active on SAI. When activating the 4 MHz bit-clock on SAI1_SCK_A, Vref and temperature measurement become very noisy, while externally connected ADC inputs are not affected.See attached graph for differ...

STM32H743ZI adc + bdma no callbacks

Hello every body, It is my first post and I´m newvy with this tecnology. I'm trying to read from adc 1, 2 and 3 values from the DMA (in case of use adc 1 and 2) and the BDMA (case adc3). In the two first cases, the interrupts are generated correctly ...

Captura.PNG Captura1.PNG Captura2.PNG

STM32F105 64 pin bootloader

Hello I have been asked how difficult it will be to create a custom bootloader for the STM32F105.We are for some reason using the 64 pin version of the chip and from the AN2606 i can see """""Workaround• For 64-pin packagesNone. The bootloader cannot...

sklindt by Associate II
  • 6836 Views
  • 11 replies
  • 3 kudos

stm32G474re adc performance

ADC analog bandwidth tests:--board nucleo-G474re, on-board voltage reference.--sampling rate 2.8 msps, free-run mode, 12-bits, --156 kHz & 19.47 MHz.  Approximately at 19 MHz ADC has ENOB < 6 bits, limiting factor seems to be aperture jitter about 12...

156.25kHz-3.jpg 19.47MHz-3.jpg adc test circuits.png
MasterT by Lead
  • 9476 Views
  • 7 replies
  • 2 kudos

HAL_I2C_IsDeviceReady() returning HAL_BUSY

Hi, I'm using an STM32F401RE board for a class(programming using MacOS). Right now, I'm using VSCode and make to edit and compile my code, then using stlink to flash it. Now, I'm trying to communicate with an MPU6050 using I2C; however, when I run HA...

AllanLiu by Associate II
  • 9078 Views
  • 8 replies
  • 2 kudos