User Activity

Hi, I am using the STM32ubeMX v6.14.0 to generate a USB-PD DRP following the link below:https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_RoleI noticed that when I set the CubeMX to have mor...
Hi, I'm using the code generated by CubeMX ver 16.14.0 following the following link to develop a USBPD sink. https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_RoleI added an APDO to the PDO ...
Hi, I am using the STM32CubeMX ver 6.13.0 to generate a USB-PD DRP application. After generating the code following this procedure for custom boards (https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Deli...
Hi, I am using the STM32G0B1CBTX with STM32CubeMX ver 6.13.0 to produce a USB-PD DRP application. So far, I managed to implement a USB 2.0 Host as this is also needed. When trying to add the USB-PD DRP following ST-s tutorial BUT omitting the inclusi...
Hi, I am using an STM32G0B1CT6 and generated code using the STM32CubeMX to use the USB Host library to interface the CP2112 device. I am able to enumerate and communicate with the device using the interrupt IN/OUT. I am also able to get reports using...
Kudos from