STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747 Custom Board Firmware Loading Problem

Hi Madam/Sir,We recently developed a custom board using STM32H747. The designs and schematic were based on Portenta H7 and the disco board. We received the board from PCBWay and confirmed that hardware-wise, it's okay and was proven electrically corr...

IMG_20231103_135523_217.jpg Screenshot 2023-11-07 103045.png Screenshot 2023-11-07 102855.png Screenshot 2023-11-07 102837.png

Purchase from www.avaq.com

How are parts purchased from www.avaq.com?We want to purchase the stm32 series, this one https://www.avaq.com/chip/stm32l010f4p6Looking for some advice. 

I2C and SWD connected wrongly

Hi,I ordered a PCB and after I had soldered all the components I noticed that in the PCB there was a connection between my SWD interface to I2C pins (PF0, PF1) and SWD pins were connected to the I2C bus. I tried short-circuiting them with a tiny copp...

JS8 by Senior
  • 2117 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H7B3I Timer 1 - Software intiated One Pulse Mode

Hi, I wish to produce a single pulse; lo-Hi delay Hi to Low. I am using Timer 1 PB15 which is the complementary output timer Channel 3I am using the timer in the following sequenceTimer initialisationSet the ARR and CCR3 with the followingARR = 2241 ...

Wakeup from standby with Wakeup Pin

Posted on June 25, 2014 at 13:00 I want know if is possible to wakeup the MCU(STM32F4) fromstandby power mode with only the Wakeup pin, without setting the RTC allarm. i have try this but the MCU don't wakeup. HAL_EnableDBGSta...

STM32U585 I2C SCL remains low and I2C hangs

Hi,I have two STM32L0 (slave) and STM32U585 (master) MCUs. I have no issue when Slave transmits data to Master. But, if Master transmits signal to Slave, it sends all the 9 clock pulses with address bits, but then the SCL remains low while SDA return...

ashah.16 by Associate II
  • 2912 Views
  • 4 replies
  • 0 kudos

stm32f103 startup io initialization problem

hello.this is the first time I've had this problem , I describe this problem next:1 the io initialization input is normal (this is the feature I want)2 when I power off and restart, I find that the same pin initialization input is not responding3 rep...

shan chen by Associate II
  • 3427 Views
  • 4 replies
  • 0 kudos

Resolved! Calculate caps for LSE crystal oscillator

hi,i am using a ECS-.327-9-34QCS-TR with a 1.5pF caps on a STM32H743BIT6.I want to know the exact method to calculate the right value for the oscillator caps.because my RTC is off by 5mSec.