STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750 FMC + LCD

I’m having some trouble related to using the FMC to interface with a LCD. We are using NE1 as chip select, LCD register select is A0, 16 bits of data.  When I’m scoping the signals, I’m seeing the A0 go high during 16 bit writes to 0x60000000 (comman...

SMoon.2 by Associate III
  • 8076 Views
  • 5 replies
  • 0 kudos

Resolved! AES v SAES

Hello,The STM32U585 Reference Manual say these chips have one AES and one SAES peripheral. In turn each of these have an "AES core algorithm (AEA)" component. I expect that to mean that there are two physically independent AEA's on the chip. Is that ...

EC.3 by Associate III
  • 2083 Views
  • 1 replies
  • 0 kudos

Resolved! How to recover continuous data with DMA ?

Hello,I have a program that works in DMA but I would like to put a function to know when the transfer in the DMA is finished so that I can recover the data continuously. Do you have any information on this ? Here is part of my code  HAL_SAI_Register...

DYann.1 by Senior II
  • 6742 Views
  • 11 replies
  • 3 kudos

STM32 DFU protocol DFU_UPLOAD problem

Hello,I am trying to implement the DFU protocol in an Android app. I am following AN3156.I am using UsbDeviceConnection class for the control transfer in android. I am able to write to the memory to any address using the routines described in AN3156 ...

LLope.31 by Associate III
  • 6580 Views
  • 7 replies
  • 4 kudos

Resolved! ADC output ranging about 2000 up to 4095

I'm running an STM32L452RCTX uC, and I'm trying to implement a 2.5Vref+ ADC.Things weren't looking quite right on the pins I intend to implement, so for now I'm driving a floating TP with a power supply so I can directly test input vs output.When dri...

APTT_0-1701355234848.png APTT_0-1701354855868.png APTT_1-1701354898880.png
APTT by Associate II
  • 7303 Views
  • 16 replies
  • 2 kudos

QSPI DTR Mode

Hii,Can someone please help me out in configuring QSPI in DTR mode to read and write data to the external QSPI memory. What all configurations are required to change to switch from STR to DTR? I am using STM32F469xx MCU with MT25QL128ABA NOR Flash in...

Resolved! Help for choosing UART pins for bootloader

Hello,I'm designing a pcb with a STM32L031 MCU. I will use serial UART2 for bootload and debug.In ST application note nº2606 and "STM32L031x4 STM32L031x6 datasheet", it is said :"The boot loader is located in System memory. It is used to reprogram th...

Arthur21 by Associate
  • 3984 Views
  • 6 replies
  • 3 kudos

INA1863IDCKR

Hello,I am trying to read the value from the INA186A3IDCKR current integrated circuit using the ADC2_INO channel on the stm32f103c8t6 microprocessor. My ADC channel is connected to the Vout section. When I examined the datasheet, I did not come acros...

rl.png
Leylifer by Associate II
  • 3925 Views
  • 5 replies
  • 1 kudos

RF shielding / leakage problem

We have one of our products failing a certification test because the radiated RF energy at 168 MHz is too high. This 168 MHz being the MCU clock frequency. The treshold is only exceeded by 0.8 dB so that's really annoying. We could solve this by plac...

RHarte by Associate II
  • 947 Views
  • 0 replies
  • 0 kudos