2023-08-14 7:39 AM
Hi
We are using the DISCO-L072CZ-LRWAN1.
USART-5 uses pin PB3 for Tx, is this pin not available on the LoRa development kit ?
Is there a way to re-route the USART-5 Tx pin or access it ?
thanks
Solved! Go to Solution.
2023-08-14 8:40 AM
2023-08-14 8:40 AM
2023-08-14 9:13 AM
Once upon a time I made a post highlighting all the pins, but the forum transition seems to have destroyed that. There are about 3 escapable UART as I recall. You might have to split a UART to get both TX and RX from different ones.
There's a finite number of pins on the WLCSP and escaping from the Murata module.
PB3 is used internally for the Radio's SPI connection
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.