STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Best Developement Platform for Startup

Posted on February 13, 2013 at 00:04Hi All,We are a new startup and have a proof-of-concept device going on a STM32 being coded in the Keil IDE. However, we are using their evaluation copy which only permits 32KB max program size and we have surpass...

Logging debug data with KEIL uVision.

Posted on January 11, 2013 at 20:29Hi.How i can get runtime data out of SMT32? The need is to analyze and tune filter outputs and overall process. Currently I am using SMT32 discovery board. And my development tools are Keil uVison v4.6 with ST link...

glcd custum configuration on stm32f407vg

Posted on October 10, 2012 at 07:49Hello everyone! I am using a customized board in my lab for building my application. the board has some function buttons and a 320x240 Graphical LCD with touch panel. I will be using Keil MDK 4. Initially, I need t...

STM32F0Discovery timing issue

Posted on August 29, 2012 at 17:11 I am trying to have a simple millisecond delay function and experiencing some very strange results. I am using Keil uVision V4.00.0. Here is my code: #include ''stm32f0_discovery.h'' //prototypes v...

rl-usb with audio device class

Posted on August 31, 2012 at 10:07Hello every body,I try to implement on my stm32f4-discovery a program with usb audio class to make windows use the board as speaker.I worked on keil 4.54 and rl-usb under windows seven x64.The problem is the followi...

STM32F4 discovery and Keil + GCC

Posted on August 06, 2012 at 15:25Can anyone give me exact steps to use STM32F4 Discovery - M4 board with, Keil and GCC? I am not able to download it (I am new to ST too, but I want to do some programming with GCC on M4) via ST_LINK, it says could n...

prasanth by Associate
  • 295 Views
  • 1 replies
  • 0 kudos

Which files to use? CMSIS from Keil of ST?

Posted on June 08, 2012 at 10:31I would like to apologize if this topic is already been discussed, but my search just wasted time.We are trying to figure out which files to use for our ST device (STM32F2xx).We would like to use the ST standard perip...

cameronm by Associate
  • 563 Views
  • 5 replies
  • 0 kudos

STM32L EEPROM HARD WRITING

Posted on December 23, 2011 at 07:33Good day! The controller has a built-in EEPROM, which is very easy to program by software. It don't suit me. Can I program it during pouring code via the programmer(JLink)? I use Keil4.21 #eeprom #jlink #keil

fiim by Associate III
  • 375 Views
  • 2 replies
  • 0 kudos
Labels