User Activity

Hello! I once asked a question about ADC:("adc-functionality-in-stm32f1-stm32l15x-series")Since then, the ADC has gotten much,much better, thank you!There are even versions with 16-bit. But there is still one serious problem. This is a built-in refer...
Posted on November 13, 2014 at 19:03Hi all! I am interested instm32F37. They are notproduced inthe bodyQFN24thatI need. (Or my special design.) Can you producethis design, what is the minimum number.
Posted on July 22, 2013 at 09:36Hellow! (stm32f37)�?�ow would you organize Switch between Mass Storage and Custom HID in Composite project? Where is the variable, changing which can be initialized either hid or mass storage or together?
Posted on April 19, 2013 at 16:49VDDC should be 5uA, AVDD should be 2uA. But I have 500uA.  I tried to enter in the stop mode before and immediately after the system_init, without any initialization settings. Tried also to do pins IN, FLOAT, AF. Sto...
Posted on December 23, 2011 at 07:33Good day! The controller has a built-in EEPROM, which is very easy to program by software. It don't suit me. Can I program it during pouring code via the programmer(JLink)? I use Keil4.21 #eeprom #jlink #keil