STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Incorrect Flash Size

Hello. I am confused about the amount of flash on an STM32F105VBT6. From the overview for the STM32F105/107 devices, I gather that this MCU should have 128 Kbytes of flash. And in STM32CubeProgrammer, in the lower right, it says that the target has 1...

John54 by Associate II
  • 3181 Views
  • 4 replies
  • 0 kudos

Configuring NUCLEO-H755ZI-Q at 480MHz

I'm trying to configure NUCLEO demo board at 480Mhz but I'm not able in any way, the following clock configuration seams to be correct, no conflictsBut the code will permanently hang on on the following configuration lineIf I comment the line while(!...

0690X00000DXYieQAH.png 0690X00000DXYijQAH.png 0690X00000DXZ6vQAH.jpg
GMG by Associate III
  • 12266 Views
  • 14 replies
  • 3 kudos

STM32L0x3 Interrupt Latency

Good morning,I am working with a board mounting a STM32L0x3 microcontroller. My SystemCoreClock is 32 MHz and TIM12 is clocked at 4 MHz. TIM12 has been configured in order to work in Capture Mode on Channel 1 (falling edge).The ISR does what is liste...

Dave94 by Associate II
  • 8173 Views
  • 14 replies
  • 4 kudos

MCUs: We want your knowledge base suggestions!

Dear community members,We invite you to provide your suggestions for knowledge base articles in this thread. We strive to create articles that can assist or inspire you in the best possible way. Anything goes, the only condition is that it is related...

Resolved! PWM DMA stops after 2 pulses when preload is disabled, (does not when compare register preload is enabled)

I am experimenting with PWM DMA on STM32F407VET6. The code creates pulses of increasing width.If I enable the output compare preload, the number of pulses is 2 instead of 6.The first pulse at startup is the default setting from the configuration in M...

_legacyfs_online_stmicro_images_0693W00000bida9QAA.png _legacyfs_online_stmicro_images_0693W00000bida4QAA.png
Johi by Senior III
  • 4625 Views
  • 9 replies
  • 0 kudos

Resolved! STM32L462 Load Capacitors

Hello, I am using an STM32L462 microcontroller with a crystal from Wurth: 830 016 178This crystal has a load capacitance of 6 pFI calculated the two load capacitors CL1 and CL2 to be 4.3 pFNow, everything is working OK, and the RTC is running fine......

Resolved! Record audio using DFSDM and send the data over UART

I have a B-L475E-IOT01A2 board. I'm trying to use the onboard microphones to record audio, using the DFSDM peripheral, and then send the data over UART to my PC to play it back. The thing is, the data I get is basically just static.Here is how I conf...

anwvo by Associate II
  • 4911 Views
  • 6 replies
  • 1 kudos

Find STM32 with 5 encoders input timers,

For a project, I need to find a stm32 that has a minimum of 5 timers that can read encoders, and it has to have a CAN-bus peripheral.Is there a way to do this in the part selectors? I can select the minimum number of 16bit timers, but not all 16bit c...

Vidicon by Associate II
  • 7377 Views
  • 17 replies
  • 8 kudos

Resolved! STM32H743VI FDCAN didn't works as classical CAN

Hello, I have some trouble with FDCAN.Please let me know what is wrong with my settings. 1. Current problem: My STM32H7 transmit only error. (Logic Analyzer) (PCAN View)Same error signal repeat endless and if I connect PCAN, many other error and stuf...

LSH_6-1707659672665.png LSH_0-1707657852549.png LSH_5-1707659199679.png LSH_1-1707658358071.png
LSH by Associate II
  • 5437 Views
  • 5 replies
  • 6 kudos