STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C transmit error by I2C_FLAG_AF flag

Hi all,I want to drive Humidity and Temperature Sensor SHT4x(address is 0x44).I finished the driver code in STM32F103C8 with HAL lib, but when I used the same driver code in STM32F429IG with HAL lib, the HAL_I2C_Master_Transmit() always returned HAL_...

Junde_0-1708322372777.png Junde_1-1708322646196.png
Junde by Senior III
  • 2555 Views
  • 1 replies
  • 0 kudos

Resolved! Stm32H743 spi function question

I developed with the stm32f756 chip and then switched to the stm32h743 chip.Then, the functions "LL_SPI_TX_FIFO_FULL", "LL_SPI_IsActiveFlag_BSY", "LL_SPI_IsActiveFlag_TXE", and "LL_SPI_IsActiveFlag_RXNE" that were in "stm32f7xx_ll_spi.h" cannot be fo...

ToonToon by Associate
  • 2801 Views
  • 4 replies
  • 5 kudos

Resolved! Can't find HAL_UARTEx_GetRxEventType() in STM32L4xx HAL code

Hi folks,I use CubeMx to generate UART∕DMA code for STM32L4xx MCU.CubeMx uses currently latest STM32Cube_FW_L4_V1.18.0 package, but HAL_UARTEx_GetRxEventType() is not included in it, neither HAL_UART_RXEVENT_* events.I found it is included in the lat...

Lex by Associate III
  • 1840 Views
  • 1 replies
  • 1 kudos

Resolved! HAL_UARTEx_ReceiveToIdle_DMA() timeout

Hi folks,I'm using HAL_UARTEx_ReceiveToIdle_DMA() on STM32L4. If I use minicom and type a few characters, HAL obviously detects an idle state after each single character I typed.I'd like to configure a idle timeout value used in HAL_UARTEx_ReceiveToI...

Lex by Associate III
  • 2467 Views
  • 2 replies
  • 1 kudos

Resolved! Failed to execute MI command load *.elf - NVIC - Error STM32G0B1?

Hello.I encountered strange CubeIDE behavior on a customer board with an STM32G0B1CEU.I've found similar glitches on this forum, but they mostly stemmed from fake HW.I use all original STM from MOUSER.If I enable PWM on TIM4 in MXcube, without NVIC, ...

RinGO by Associate III
  • 5309 Views
  • 3 replies
  • 0 kudos

Resolved! Input capture not detecting square wave

I have built a sine wave to square wave circuit and now want to measure its frequency with the STM. I can see on the oscilloscope that the circuit works, however I can detect neither a rising nor a falling edge with the chip. It is not a problem with...

waves.JPG
Qwyntex by Associate III
  • 5944 Views
  • 11 replies
  • 0 kudos

Resolved! Bus fault Accessing flash

Hi,MCU- STM32H7I get a busfault exception when I read bank2 flash memory. I can read bank1 with no issues. From the flash register SR2, it shows as ECC double bit error. This is new pcb and I can flash the hexfile to bank1 successfully. Even a Jlink ...

andy_long_0-1708033978473.png andy_long_1-1708034440760.png
andy_long by Associate III
  • 4809 Views
  • 7 replies
  • 2 kudos