cancel
Showing results for 
Search instead for 
Did you mean: 

G431KB abnormal current consumption

gigikw
Associate

Suddenly the CPU has started to absorb 160 mA. At the beginning, when I started using it, it was 30 mA. I cannot understand the reason. No hardware modification has been operated. Has anybody experienced anything like this? Thanks in advance.

@apoggiali 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Show enough of your schematic as to be helpful.

It could be due to external loads, or that the supplies are not connected properly, creating internal current paths and some other failure mode has been induced.

Have you changed the code? Could it be running faster? Could you be driving a pin which is being driven by some other part of your circuit? Could you have damaged the IC with large voltages for other parts of the circuit or equipment attached to it? Shorted the board on a bench or conductive surface?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..