cancel
Showing results for 
Search instead for 
Did you mean: 

Why need manually __enable_irq() after Bootloader jump to application

doushicai
Associate

Hi,

I have a bootloader used 3 years ago on 2020 on STM32F437 and it works perfectly.

This year, I am trying to use the same bootloader on STM32F205 but got problem that after the jump, the Application is not running.

After a long time debugging I found the Application is stuck in HAL_Delay()and osDelay(). 

So, I manually added the __enable_irq() in the beginning of the Application code and it magically works.

I know I have __disable_irq(); in the Bootloader code but the problems really confused me are:

  1. Why I need to manually add the  __enable_irq() in the Application code? My Application code can work alone, So, should all the necessary interrupts be initiated and enabled again in its own default generated initiate code after the jump?
  2. Usually, this kind problem is cased by the VECT_TAB_OFFSET, but I am sure I defined it correctly in the system_stm32f2xx.c 
     
  3. Why the same bootloader worked on the CubeIDE projects 3 years ago? but with the new IDE, I have to manually add the __enable_irq() in Application code?  I am using STM32CubeIDE 1.13.2 now and not a big fan of it since I get lots of old projects cannot compile in this most up-to-date IDE. This was not happened in my past CubeIDE updates. Is this the problem also caused by the new behaviors and new libraries of this new IDE?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

You don't have to use __disable_irq() at all. What you NEED to do is stop all the *** you have running that's causing interrupts at a peripheral level, because the RAM and all the peripheral instances in it are going to be completely remapped via the new app and how the linker allocated the resources, and then likely zero'd or initialized. If you do the appropriate tear-down this isn't going to be an issue, and you won't get Hard Faults.

The MCU doesn't come out of reset with IRQ's disabled, IRQ's are enabled, there's just nothing in the NVIC and none of the peripherals are banging off interrupts. Code built in startup.s and beyond doesn't expect the IRQ to be disabled at an MCU level. You will need to enable them if you disabled them

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Christian N
ST Employee

Hello Doushicai,

Thank you for contacting STMicroelectronics. Your inquiry is being escalated for specialized support.

Kind Regards,

Christian

ST Support