STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sprintf not working when ADC started

I'm trying to send ADC results over to a receiver via UART, but somewhy the program freezes on sprintf() IF I have called HAL_ADC_Start_DMA() before. If I call sprintf() before HAL_ADC_Start_DMA() it works fine. However, I need to call it after start...

JS8 by Senior
  • 5103 Views
  • 10 replies
  • 0 kudos

Resolved! SCKL frequency of SPI

Hello,I have set the BR bit in CR1 to 0 with the expectation of obtaining an 8MHz clock frequency. However, I am encountering an actual frequency of approximately 1.042MHz. Does anyone have an explanation for this issue, or should I consider implemen...

Resolved! STM32F042F6P7 (TSSPOP20 package): CAN availability on CubeMx

Using STM32CubeIDE (v1.14.0) with STM32F042F6P7 (TSSOP 20) to configure CAN pins on custom board. However the CAN peripheral is grayed-out when I open the IOC file in STM32CubeIDE. For pin assignments, PB8 is available for CAN rx but CAN tx is not sh...

hexdecimal number to send UART

Hi,I wanted to send hexadecimal numbers through UART. I am using STM32F405. Can it be done.If I am sending float number as 1.3456 string (text) to windows COM port to  english language windows application field. If for example regional settings being...

cjaya.2 by Associate II
  • 2295 Views
  • 3 replies
  • 1 kudos

Example script/program for I2C bootloader commands

Hi, I'm using a STM32G07x1 that will need to receive firmware updates from an embedded Linux CPU. The only connection between these devices is an I2C bus so I plan to use the ROM I2C bootloader to handle updates.I am aware of AN4221 that describes ho...

Resolved! STM32F413VGT6 DMA is triggered but no data is copied

Hello,I'm trying to use DMA with an Usart to receive incoming data in a circular buffer. Basically this is my code for configuration using UART5. I can send data, so i assume, that port und clock configuration is correct. When receiving data, NDTR is...

NHand by Associate II
  • 2078 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F407VGT6 Ethernet Module: Jambo frame feature?

Hi developers,   I'm new to STM32 MCU, but recently need to use it for a automotive Ethernet board design. The ethernet PHY I am going to use supports the jumbo frame up to 16kByte. Do anyone happen to know if STM32F407VGT6 can also support this jumb...

axdwqerf by Associate
  • 1616 Views
  • 1 replies
  • 1 kudos

Resolved! SPI dma reads start at index 1 after first read

I'm trying to read and write SPI bytes from an STM32F446RE chip with DMA.  The STM32f4 is the slave and a RPi is the master.  The first SPI read works fine (data read into buffer starting at index 0), but subsequent reads have the data starting at in...