STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F407VGT6 Ethernet Module: Jambo frame feature?

Hi developers,   I'm new to STM32 MCU, but recently need to use it for a automotive Ethernet board design. The ethernet PHY I am going to use supports the jumbo frame up to 16kByte. Do anyone happen to know if STM32F407VGT6 can also support this jumb...

axdwqerf by Associate
  • 1615 Views
  • 1 replies
  • 1 kudos

Resolved! SPI dma reads start at index 1 after first read

I'm trying to read and write SPI bytes from an STM32F446RE chip with DMA.  The STM32f4 is the slave and a RPi is the master.  The first SPI read works fine (data read into buffer starting at index 0), but subsequent reads have the data starting at in...

Resolved! stm32g030 RTC/LSI ticks 50% too often

Hi!I use the RTC of a STM32G030K6T. It is clocked by LSI (appr. 32kHz). And PREDIV_A is 0x0 and PREDIV_S is 0x7FFF. So I expect that RTC_SSR overflows every 1.024sec...But: It overflows every 0.687sec... As if the LSI frequency would be 47712Hz...I m...

RRIDDICC by Associate III
  • 2202 Views
  • 4 replies
  • 2 kudos

Resolved! DMA1 Stream7 DMA2 Stream7

Hi I m using SPI DMA on H7 series, and notice under SPIx_TX and SPIx_RX there are at least 14 DMA channels to choose from, i.e DMA1 Stream 0-7 and DMA2 0-7. Can i select these "channel"  randomly or is there a reference manual that state otherwise? L...

Resolved! STM32 H5 I3C CCC transmit

I used STM32H563 transmit a message through I3C CCC direct.I create a new CCC command "0xA0".Control send the command to target.But target will enter HAL_I3C_ER_IRQHandlerUesd the general command "0x89".The target can receive this command. The Buffer...

Sunwaz_0-1708916889390.png
Sunwaz by Associate III
  • 4071 Views
  • 8 replies
  • 0 kudos

STM32U5A5: SAI1 as PDM MIC interface

Does anybody have an example code how to use SAI in STM32U5A5 as PDM interface?I use STM32U5A5, with LQFP64 package. So, I understand from datasheet: the SAI (I have just SAI1 available om pins), supports PDM interface (for MEMS MICs). My package has...

tjaekel by Lead
  • 1649 Views
  • 1 replies
  • 0 kudos