STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Writing data to STM32G4 Flash

Sorry, my first time programming an STM32.  I have a bunch of data I need to store for a few hours, and the thought was to store it in Flash since there's a lot more of it (512k vs. 128k for regular RAM) but it looks to be pretty daunting. I've been ...

Resolved! STM32H723ZGT6 will not reboot after powering off

Hello All,I designed and built a bare metal board with an STM32H723ZGT6 and it runs fine.I have blinking LED's, timer / interrupts running, HSE and LSE etc.I have been trying to figure out why if I toggle the power supply the device will not boot up ...

MDeac.1 by Associate III
  • 2986 Views
  • 4 replies
  • 0 kudos

STM32F756VGH6 register based interrupt syntax.

Hi,I am a beginner in STM32 programming. I chose purely register based programming approach without using HAL as I find it a bit harder and slower but more contributing to the overall system performance in the long term code writing skills. This time...

Vilius by Associate III
  • 6377 Views
  • 8 replies
  • 4 kudos

Resolved! UART data receive acknowledgement

Two devices A & B are communicating on UART. A sends data stream to B. B sends one byte data back to A to acknowldge that data has been received. I want to implement if A doesn't receive acknowledgement from B then it display Error message on LCD.Ple...

Nico3 by Senior
  • 3309 Views
  • 4 replies
  • 2 kudos

stm32l072rz higher stop mode current then stm32l072rb

Hello,we have a validated project based on the stm32l072rb (FLASH 128KB) microcontroller and in stop mode the entire system consumes 3.5uA.We have updated to the stm32l072rz (FLASH 192KB) and the stop mode current raised to 23uA. In standby mode both...

Resolved! How to check the authenticity of STM32 chips?

Hi everyone, I'm deep into developing a project that is not only a passion but also a venture I'm financially invested in. I recently ordered a small batch of 50 PCBAs equipped with STM32L476RET6 microcontrollers from a well-known Chinese manufacture...

STM32L476RET6.JPG
AChap.1 by Associate III
  • 5603 Views
  • 6 replies
  • 5 kudos

stm32wb55 ADC read error

Hi all,I am using an stm32wb55 neucleo board for a wearable based project. I am using ADC1-IN1 to read the adc raw value from MCU pin PC0 of wb55 board.  A voltage divider circuit was connected to scale down the BAT voltage from (4.2-3.7) to (1.8-1.5...