STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Receive stuck

Hello everyone, I am trying to communicate with lora e5 using usart1, when i send "AT\r\n" command and i try to receive data from the same uart(lora) the function while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status) blocks the execution...

SIP VOIP

Hello guys, is there a SIP library for VOIP or an example of a project without using other third party libraries for VoIP? Thankyou in advance

rizki27 by Associate
  • 2279 Views
  • 1 replies
  • 1 kudos

SMBUS Block write -Block read process with Middleware

Dear expertI am currently implementing the SMBUS communication with TI BQ40Z80 via STM32L431xxx + Middle ware.However, when observing the smbus waveform, N byte block write does not work properly and block read is also strange.Other register accesses...

kim1 by Associate II
  • 1934 Views
  • 0 replies
  • 0 kudos

STM32H753XI LWIP + MDMA

Hello, we're using STM32H753XI in our custom board wherein we've ADIN1200 LAN driver, W25Q flash on QUADSPI. we've configured the memory regions for Ethernet Rx, TX DMAs and pool memory like this       RW_DMARxDscrTab 0x30040000 0x60 { *(.RxDecrip...

AShel.1 by Associate III
  • 2834 Views
  • 4 replies
  • 0 kudos

Issue with reading i2c eeprom memory with Nucleo-F446

Hello all .  I have been working for days to make nucleo f446re reads i2c eeprom .  The i2c eeprom am trying to read uses 0x78 address as the slave address .  I tried use the Nucleo-64 f446re with stm32 cube ide using IsDeviceReady in hal i2c . And i...

adelsaeed by Associate II
  • 3045 Views
  • 4 replies
  • 3 kudos

Resolved! SPI communication with 3 wire display

Hi community,I have a display, which has only CLK, DI and CS pin for SPI communication. It uses TI protocol.The original driver is only working with raspberry pi, I try to import it into my custom STM32 MCU board, the CLK and CS signals seem okay,  O...

Danny0007_1-1708464524960.png Danny0007_2-1708464622941.png

Resolved! Writing data to STM32G4 Flash

Sorry, my first time programming an STM32.  I have a bunch of data I need to store for a few hours, and the thought was to store it in Flash since there's a lot more of it (512k vs. 128k for regular RAM) but it looks to be pretty daunting. I've been ...

Resolved! STM32H723ZGT6 will not reboot after powering off

Hello All,I designed and built a bare metal board with an STM32H723ZGT6 and it runs fine.I have blinking LED's, timer / interrupts running, HSE and LSE etc.I have been trying to figure out why if I toggle the power supply the device will not boot up ...

MDeac.1 by Associate III
  • 2973 Views
  • 4 replies
  • 0 kudos