STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f446re with E22t900d

Firstly, hello, I currently have the Nucleo-F446RE and E22t-900d LoRa module. First of all, how do I connect these two products? Then, how can I send the data I receive via the stm32 card to another LoRa module connected to the USB port of my compute...

gazili by Associate
  • 751 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F7 and STM32H7 HDMI implementation

Hello,Please forgive me for what is probably a newbie question.  What is required to implement an HDMI interface with the STM32F7 or H7 MCU series?  Is a DSI-to-HDMI bridge always required?  What is the max. supported display resolution?Thanks,Scott

Resolved! Does NUCLEO-IKS01A1 support I3C? (with NUCLEO-H503RB)

Hi, I'm trying to check I3C protocol with NUCLEO-H503RB and IKS01A1.I just followed below link for I3C. https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3CAnd I can see that the master transmit the data but there is no ACK from the slave.(I've...

Resolved! STM32 RTC3 Mixed Mode: Writing TR resets SSR?

RTC3 of some newer STM32s introduce a RTC mixed mode, where both binary part (32-bit down-counting sub-seconds register SSR) and classic BCD calender (TR/DT) mode are operational.In my case I am using this for classic style BCD alarms together with b...

Resolved! FDCAN Bootloader for STM32G0B

I did not find any solution of Bootloader for CAN2.0A or CAN2.0B with SMT32. Currently i am using below part no. MCU-'STM32G0B1CCT6' CAN IC-'ISO1044BD'

Pooja321 by Associate II
  • 4185 Views
  • 7 replies
  • 1 kudos

CMSIS DSP CFFT incorrect frequency analysis

hi, I'm trying to do the FFT using the CMSIS DSP V1.15.0 libraries but I get a graph with random frequencies...I have a CM4 microcontroller(without FPU) I implement the below code and get random frequencies.I test the same code on a CM7 microcontroll...

Mavi by Associate II
  • 1967 Views
  • 1 replies
  • 0 kudos

Resolved! WWDG early wake interrupt to prevent reset

Hi,I have a question regarding the possibilities and best practises of the early wake interrupt generated by the window watchdog.Is it possible to use the EWI to refresh the watchdog? And if so, is it actually a good idea and reliable?To describe the...

StefanR by Associate II
  • 2396 Views
  • 3 replies
  • 1 kudos

Resolved! Flash STM using 1 USB - STM32H755

Hi there, I am working on a project using the STM32H755 zi that has 1 USBC port, can we use the same port for uploading the code, UART Communication and powering the device instead of using ST-LINK? Or is there any way to use ST-LINK for communicatio...

isaacjack by Associate II
  • 1526 Views
  • 2 replies
  • 2 kudos

Resolved! STM32F4 Enabling and Disabling SPI using Timer or DMA

Hello, I'm using the STM32F469NiH6 to try and do a certain number of SPI transactions (let's say 12 bytes) at regular intervals without core intervention, using Timers and DMA. And I have a couple of questions concerning this (I have had a look into ...

ribdp by Associate II
  • 3585 Views
  • 5 replies
  • 2 kudos