STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer with a relax period

HII need a simple timer that can make a PWM signal BUT with custom pauses or a relax period every number of pulses ... I have the code working very well with no relax , but I do not know how to write the relax period in the timer script itself...Here...

Search for the MCU

Hi,1, Im searching for an mcu which can handle a HS/FS communication(sends data to PC 50*8830bytes) with a PC, and an USB fs communication with a external 4 port hub. the hub will connect 4 stm's which sends data(1316 bytes) periodicaly and sincroniz...

RBacs.1 by Associate II
  • 979 Views
  • 2 replies
  • 0 kudos

Resolved! UART fired only once - STM32U5 Custom Board

Hello,I'm working with an STM32U5 custom board.I use the LPUART1 to read input with an interrupt as shown below and to write it back on the same LPUART1 :  void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { HAL_GPIO_TogglePin (GPIOA, GPIO_...

TV79 by Associate II
  • 3079 Views
  • 5 replies
  • 5 kudos

OV7670 not being recognized

Hello,I want to use an OV7670 camera with my STM32U585CIU6 MCU. I've done all connections but failed to identify the camera module with I2C. I have then removed the wiring and just kept the following connections: 3.3V supply, GND, SCL and SDA (pull-u...

Resolved! STM32H753ZIT6- ALE &CLE

Hello team, I am trying to connect external NAND flash with STM32H753ZIT6. my concern is with respect to FMC_ALE and FMC_CLE pins as, in Pin no. 80 and 81 these are multiplexed with address lines whereas pin no 98 and 99 can also be used as FMC_ALE a...

How to use nucleo-h7s3l8

 Hi all,I buy a nucleo-h7s3l8 but I don't how to program and debug itH7s3l8 mcu is different from other stm32 mcu that I use beforeMy question is as followsIf I use STM32CubeMx to create project.I will get two subproject boot and appli in Stm32CubeId...

prometheans152_0-1717576760426.jpeg

Resolved! STM32F429 read from PIN to DMA

Hello everyone, I have a board.STM32F429I DISCO1, I want to read, say, two bytes of parallel data from port A{15:0}, into the DMA buffer, every time a rising edge of some signal comes to the microcontroller from the outside.How exactly can this be im...

gevmar by Associate III
  • 3458 Views
  • 5 replies
  • 4 kudos