STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to tell if interrupts are enabled

I need to determine if the interrupts are enabled at one point of my code but I have not been able to find any reference for the STM32G474.  It doesn't look like there is a PRIMASK register which is mentions in another post.I know how do enable and d...

So clock output on MDF CKI1

I am trying to provide a clock to PDM microphones using the CKI1 MDF pin, and no clock is being generated. The MDF correctly generates a clock signal on MDF CKI0. The IO configuration for CKI0 and CKI1 is the same (except for the alternate function r...

jcmoreau by Associate II
  • 1992 Views
  • 2 replies
  • 0 kudos

Bootloader OTA stm32l072

The micro STM32L072kz supports the OTA (Over-The-Air) method, I would like to perform the bootloader through the main firmware, without the need to use a USB cable or bus, write a firmware that with the help of a 4G modem downloads a new firmware fro...

Wave by Associate II
  • 1701 Views
  • 2 replies
  • 0 kudos

Resolved! Vcore voltage levels - published values in source?

Hi,What are the Vcore volage levels for the STM32H562 as applied by the VOS configuration bits? Datasheet -VOS0-3 = [1.35, 1.20, 1.10, 1.00] VSource - VOS0-3 = [1.2, 1.1, 1.0, 0.9] V The discrepancy lies in some outdated comments I think; maybe the v...

jreina by Associate III
  • 2682 Views
  • 4 replies
  • 0 kudos

N DMA Transfers based on a timer trigger

I'm trying to use timer 8, stm32f429I, as advanced timer, to do N DMA transfers, that copies data from portD to memory and it does trigger on PC6 after triggering, an N DMA transfers should be shot I have tried, but now it triggers only DMA transfer,...

Resolved! I2C Timing configuration for STM32G4xx

Hello guys,I am having problems setting the correct I2C clock on the STM32G4xx in Master Mode. The example configuration from the data sheet for 400 kHz at 16 MHz f_I2CCLK generates 432 kHz (RM0440-Rev4: P1892 Table 381). I use the __LL_I2C_CONVERT_T...

uhl by Associate
  • 2835 Views
  • 2 replies
  • 1 kudos