User Activity

Why isn't VREFBUF enable available in CubeMX for the STM32L432 series? I believe the reference manual says this series has control over the VREFBUF. It also seems there's no struct for VREFBUF control in the stm32l432xx.h file.
I'm trying to get the internal temperature sensor working on a custom board with an STM32L432KC. VDDA is 2.5V and is stable. The raw readings I'm getting are about 200 counts higher than I would expect on a 12bit config. The reading doesn't change ba...
I've been using an STM32G474xx in a project for a few years now and have a function that jumps to the bootloader. It seems in a recent rev of the chip the bootloader has changed. I'm finding that I can no longer jump to the bootloader similar to how ...
What exactly is meant by "If Boot from FLASH"?
I'm working with an STM32F217 and I have a few timer channels setup as sync clocks to regulators (around 1.5 MHz). I'm checking to make sure my sync lines are actually using HSE as a reference clock by looking at the phase drift between my external o...
Kudos from
Kudos given to