User Activity

     We are using STM32MP!57A processor in our custom board.      In this we are unable to read the internal ADC values in our cards.     Actually, we initialize the internal ADC pins in cortex-M4 core with support of STM32CUBEMX and debug in CubeIDE...
Hello     We are using STM32MP157A processor in our custom board.      Now we are implemented IWDG1 in Cortex A7 processor. The IWDG1 bit is not going to set after reset the processor with Watchdog timeout.we checked in following registers• RCC BOOTR...
Hello I have built the st-example-image-qt using openstlinux(Openstlinux-5.15-yocto-kirkstone-mp1-v23.07.26)  to run a qt application for stm32mp157f-dk2 board.I could run the application the application successfully.It would be very helpful to move ...
Hello I Want to configure HDMI support for stm32mp157f-dk2 board using Buildroot. I am actually able to run an application on display but I couldn't do it with HDMI.The version of buildroot i am working on is Buildroot 2024.05. Thanks in advanceSrika...
Hello We have built OpenSTLinux(Openstlinux-6.1-yocto-mickledore-mp1-v23.06.21) for stm32mp157f-dk2 Board and I have built st-image-weston image. Iam new to this Yocto,so I request you to help with the following:How to make changes in dts & dtsi file...
Kudos from
Kudos given to